User Activity

HelloI'm working on a 320x240 SPI LCD using partial frame buffer strategyThe number of blocks is configured to 2 and the block size is configured to 19200 bytes.The problem is that flushFrameBuffer draws only 240x20 pixels at a time, however I would ...
I'm using a STM32F469 Discovery board, i was using a board with B-01 revision, my software works just fine, now i want to use the same board but with B-03 revision but for some reason the same software doesn't work on this board.Note: B-01 rev flashe...
When I put more graphs in a swipe container on distinct pages and try to make a swipe on the graph area, nothing happens, when i do the swipe out of the graph area, it goes to the next page. Does anybody know how can i solve this problem ?
Kudos from