2022-01-12 10:25 AM
I have a STM32G071 nucleo and want to generate an arbitrary waveform on PA0 via TIM2-CH1.
I am using the HAL_TIM_DMABurst_MultiWriteStart API: it should do bursts of 3 writes to multiple registers (ARR and CCR1).
Problem is, the DMA only updates the ARR (instead of ARR + RCR + CCR1) and only once (instead of two bursts). If I change the base register to CCR1 it only updates the CCR1 once.
I see this, because I freeze the timer when the core is halted and I added breakpoints to HAL_TIM_PeriodElapsedHalfCpltCallback and HAL_TIM_PeriodElapsedCallback (and the output waveform is BS).
Normal or circular mode have the same effect.
This is the main code:
__HAL_DBGMCU_FREEZE_TIM2();
uint32_t buffer32b[6] = {10, 0, 30, 100, 0, 300};
HAL_StatusTypeDef result;
result = HAL_TIM_DMABurst_MultiWriteStart(&htim2, TIM_DMABASE_ARR, TIM_DMA_UPDATE, buffer32b, TIM_DMABURSTLENGTH_3TRANSFERS, 6);
result = HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);All the registers I checked looked fine to me.
Could this be a hardware problem?
Full code is attached below (it only sets up the HSI for 64MHz operation and configures TIM2 and DMA accordingly and then starts the TIM-DMA operation):
#include "main.h"
/* Private variables ---------------------------------------------------------*/
TIM_HandleTypeDef htim2;
DMA_HandleTypeDef hdma_tim2_up;
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_TIM2_Init(void);
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_TIM2_Init();
__HAL_DBGMCU_FREEZE_TIM2();
uint32_t buffer32b[6] = {10, 0, 30, 100, 0, 300};
HAL_StatusTypeDef result;
result = HAL_TIM_DMABurst_MultiWriteStart(&htim2, TIM_DMABASE_ARR, TIM_DMA_UPDATE, buffer32b, TIM_DMABURSTLENGTH_3TRANSFERS, 6);
result = HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
while (1)
{
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
htim2.Instance = TIM2;
htim2.Init.Prescaler = 63;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 10000;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
HAL_TIM_MspPostInit(&htim2);
}
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOA_CLK_ENABLE();
}
void Error_Handler(void)
{
__disable_irq();
while (1)
{
}
}
void HAL_MspInit(void)
{
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/** Disable the internal Pull-Up in Dead Battery pins of UCPD peripheral
*/
HAL_SYSCFG_StrobeDBattpinsConfig(SYSCFG_CFGR1_UCPD1_STROBE | SYSCFG_CFGR1_UCPD2_STROBE);
}
void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* htim_base)
{
if(htim_base->Instance==TIM2)
{
/* Peripheral clock enable */
__HAL_RCC_TIM2_CLK_ENABLE();
/* TIM2 DMA Init */
/* TIM2_UP Init */
hdma_tim2_up.Instance = DMA1_Channel1;
hdma_tim2_up.Init.Request = DMA_REQUEST_TIM2_UP;
hdma_tim2_up.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_tim2_up.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_tim2_up.Init.MemInc = DMA_MINC_ENABLE;
hdma_tim2_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_tim2_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_tim2_up.Init.Mode = DMA_CIRCULAR;
hdma_tim2_up.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_tim2_up) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(htim_base,hdma[TIM_DMA_ID_UPDATE],hdma_tim2_up);
}
}
void HAL_TIM_MspPostInit(TIM_HandleTypeDef* htim)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(htim->Instance==TIM2)
{
__HAL_RCC_GPIOA_CLK_ENABLE();
/**TIM2 GPIO Configuration
PA0 ------> TIM2_CH1
*/
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
}
Solved! Go to Solution.
2022-01-14 9:57 AM
Not watching the registers in the debugger (e.g. in half complete callback) is a good tip!
The error was that the DMA transfer direction was wrong (peripheral to memory instead of memory to peripheral).
2022-01-12 3:20 PM
> All the registers I checked looked fine to me.
Show.
Btw. you don't observe the TIM registers in debugger, do you?
JW
2022-01-14 9:57 AM
Not watching the registers in the debugger (e.g. in half complete callback) is a good tip!
The error was that the DMA transfer direction was wrong (peripheral to memory instead of memory to peripheral).
2022-01-14 2:59 PM
Thanks for coming back with the solution.
Please select your post as Best so that the thread is marked as solved.
JW