STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Correct order of using HAL_ADC_RegisterCallback function

Dear ST Community,as part of a project to capture analog microphone data, I would like to use my own callback funtions instead of hal callbacks. For this I register my ADC callbacks with the HAL function HAL_ADC_RegisterCallback as follows:/*********...

Rookie38 by Associate III
  • 1682 Views
  • 1 replies
  • 0 kudos

STM32H7 timer interrupt slightly too fast

I am using TIM2 on a STM32H7 to generate interrupts - e.g. every 1 ms. Using the formulas from the documentation, Update_event = TIM_CLK/((PSC + 1)*(ARR + 1)*(RCR + 1)), solving for ARR and using RCR = 0 we getARR = 1/(Update_event * (1 + PSC) / TIM_...

0693W00000QMxaGQAT.png
OBjor.1 by Associate II
  • 3026 Views
  • 7 replies
  • 0 kudos

RTC hours keep counting after 24 hours

Hi,I use RTC on a STM32L073. Every 12hours, I receive a date and time to set to the RTC. (Sometime, like 1% of the time) After writen the new RTC value, the RTC doesn't overflow after 23h59min59sec and keep counting without incrementing day. I can ha...

Ppeyr.1 by Associate III
  • 3112 Views
  • 5 replies
  • 3 kudos

Resolved! STM32H7 Power down sequence

About Power-Down Sequence (Device : STM32H7B0xB)​Datasheet : DS13196 - Rev 6 Page 13"During the power-down phase, VDD can temporarily become lower than other supplies only if the energy provided to the microcontroller remains below 1 mJ. " ​Could y...

Makoto by Associate
  • 1938 Views
  • 3 replies
  • 2 kudos

Multi channel ADC + SPI + I2C

I'm using STM32 NUCLEOH743ZI2 board were I have written a code which consist of Multi channel ADC using DMA with timer, SPI and I2C protocols. SPI and I2C is not working whenever multi channel ADC is enabled else SPI and I2C is working fine. We are u...

GHARI.1 by Associate II
  • 1136 Views
  • 1 replies
  • 0 kudos

Resolved! F411 System Clock Configuration with Internal Clock

I have been working F411RE Nucleo board with LL library for quite some time. I found the sample code for SystemClock_Config uses external oscillator as showed below. I wonder if there is any sample for internal oscillator. /* Enable HSE oscillator *...

HDaji.1 by Senior
  • 2374 Views
  • 3 replies
  • 0 kudos