STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f407 - Question of i2s clock frequency

Hi, I'd like to play music through i2s interface using external audio codec.Refer to "STM32F4xx Reference Manual", Below setting is needed if MCLK is enabled on 48Khz FS.PLLI2SN : 258 PLLI2SR : 3 I2SDIV : 3I2SODD : 1After I configured above, BCLK and...

SJoo.1 by Associate II
  • 4147 Views
  • 6 replies
  • 0 kudos

STM32L152VDT6 extreme current draw on power-up

I have a design in which I am using an STM32L152VDT6 processor. The first prototype boards arrived, and one of the first things I noticed was that there was a resistance of 120 ohms between VCC and GND. I knew something had to be wrong at that point....

Bolan69 by Associate II
  • 3574 Views
  • 9 replies
  • 0 kudos

Resolved! Setting Encoder functionality on STM32F407VE vs STM32F103C8

Setting the encoder functionality on STM32F103C8 is straight forward, just set the registers that's due. But on STM32F407VE it seems more tricky: using PA6 and PA7 on TIM3, if you follow what is said in the RM0090, page 616, you're not ready to go:Fu...

0693W00000QN5uxQAD.png 0693W00000QN5wAQAT.png
Echo by Associate II
  • 3337 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.