STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! G473 - PA10 I2C. Docs issue?

I have been troubleshooting a I2C device for longer than I'd like to admit. Today I attempted to configure with CUBE, and I think I've found the pin I'm using may not be compatible.PA10. Can it be used for SDA2? I thought it could based on the AF tab...

DOCon.1 by Senior
  • 3991 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G473 I2C2 pinout mistake in Datasheet

Hi,I would like to make a new electronic design with the STM32G473, using I2C2.But it seems there is a mistake in the datasheet regarding the pinout.On pin description it says:PA8 = I2C2 SDAPA9 = I2C2 CLKPA10 = I2C2 SMBAWhereas on Alternate function ...

thomas23 by Associate II
  • 3816 Views
  • 6 replies
  • 0 kudos

STM32 device marking Technical note

https://www.st.com/resource/en/technical_note/tn1433-reference-device-marking-schematics-for-stm32-microcontrollers-and-microprocessors-stmicroelectronics.pdf Nice; however, these marking schemes tend to change over time and with changing packaging s...

How to sync ADC sampling at 192K to DAC output

On STM32F407V-Disc the divisions don't work out for an 192KHz Timer trigger for the ADC, so sampling runs a bit slower or faster, the problem is that the Cirrus DAC audio chip cannot be set to match the sample rate, so I get buffer sync drift, audio ...

Robmar by Senior III
  • 3916 Views
  • 14 replies
  • 0 kudos