STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with configuration of PF2_NRST pin of STM32C011J6

Here,PF2_NRST pin (Pin Number - 4) is configured as digital input pin.And PA13 pin (Pin Number- 7) is configured as digital output.When toggling the pin PA13, getting proper voltage level 3.3 volts and 0 volt. While reading low level on the input pin...

STM32C011J6.jpg

MFRC522 LIbrary for Uart

Hey Guys , I am working with stm32l053 controller and MFRC522 . Can anybody share any link which has library for MFRC522 UART communication instead SPI.Thanks in advance.

NBhar.1 by Associate II
  • 5703 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H735RGV6 ADC Dual Interleaved Mode Single DMA

Hello Sir/Madam,I am working on STM32H735RGV6 for interleaved mode single dma. I am having problems while getting samples from the DMA controller with ADC. The problem is as the following.1. If I want to get 8192 or a smaller number of samples, there...

ErsinKuscu_0-1687347091567.png ErsinKuscu_1-1687347122125.png ErsinKuscu_2-1687347476097.png

ADC temperature drift w.r.t reference voltage

Hallo EveryoneI would like to know the internal ADC temperature drift w.r.t reference voltage in STM32U585. I already found the info. related to  VSENSE linearity with temperature in Datasheet. But i am specifically looking for temperature drift w.r....

apoorvabs by Associate II
  • 1617 Views
  • 0 replies
  • 0 kudos

problem with Internal comp in STM32G4

Hi,I have a problem with the demoboard EVSPIN32G4 and also a motor control board using the STM32G431. The overcurrent detection using internal comparator triggers below the theory (10A insteand 100A for example). I tried to use as voltage reference V...

tmaun.1 by Associate II
  • 2387 Views
  • 1 replies
  • 0 kudos