User Activity

Reference:STM32H7MCU package 1.11.1CubeIDE 1.13.1This is not a new problem but perhaps a new perspective.  I answered regarding this in a previous post but wanted to bring up anew because of the change in tack.The problem is this: After setting up an...
I have a board design using STM32H743.I am using:STM32CubeIDEVersion: 1.13.2Build: 18220_20230914_1601 (UTC) running on:OS Name Microsoft Windows 10 EnterpriseVersion 10.0.19045 Build 19045System Type x64-based PCI am debugging an implementation of A...
Stats:STM32CubeIDEVersion: 1.13.2Build: 18220_20230914_1601 (UTC) Windows 10 Enterprise I have a project using STM32H743 and Azure RTOS, ThreadX, NetX, and FileX.In the NetX portion during initialization of the netx thread, the code performs initiati...
Using STM32H743IGKx.Tools: LinuxSTM32CubeIDEVersion: 1.12.1Build: 16088_20230420_1057 (UTC)STMCubeMXVersion: 6.8.1-RC4Build: 20230419-1431 (UTC)When setting up the SDRAM configuration in MX, I end up with a couple of signals that look like they are n...
I have a project that uses the ModuleX middleware and has been included into the build.  However, I am stuck trying to figure out how to create a sub-project to build the Module code.  Thought that might be in the New>STM32 Project wizard but it alwa...
Kudos from
Kudos given to