STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431 - how to use interrupts within library

Hi,I'd like to create a library for fast handling the USART2 and TIMER. Unfortunately, when I move the USART2_IRQHandler() to the library, the linker do not include this function in a final application, and the program crashes by ending up in the end...

mrox by Associate II
  • 4103 Views
  • 5 replies
  • 3 kudos

USB VCP Packet Loss with STM32L4R and Windows

Hello, I have an STM32L4R9ZI controller connected to a computer running Windows 10. I have a custom protocol where the computer sends a command and my controller responds. I am using VCP to achieve this. The communication is established and operation...

Makarand by Associate II
  • 2644 Views
  • 3 replies
  • 0 kudos

Resolved! PC3_C as input

I use PC3_C pin as an GPIO_Input, but when i debug it is flickering between 1 and 0 even without any connection to the pin. anyone knows what happened?this is the setup i useGPIO_InitStruct.Pin = Emergency_Pin;GPIO_InitStruct.Mode = GPIO_MODE_INPUT;G...

BAl K.1 by Associate III
  • 2188 Views
  • 2 replies
  • 0 kudos

Resolved! 1.8V Power Supply on STM32H735

Hello, I'm designing a board based on the STM32H735IGK3 microcontroller in which I want to include two HyperBus / OctoSPI memories in multiplexed mode. For this kind of memories there is more avaiblity on 1.8V power supply, but reading the documentat...

vmartinm_0-1689594028152.png
vmartinm by Associate II
  • 2370 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4 - are pullups during reset active when RDP level is 2?

Citing from the STM32L431 manual:The debug pins are in AF pull-up/pull-down after reset:• PA15: JTDI in pull-up• PA14: JTCK/SWCLK in pull-down• PA13: JTMS/SWDAT in pull-up• PB4: NJTRST in pull-up• PB3: JTDO in floating state no pull-up/pull-downLet's...

ramses946 by Associate III
  • 1850 Views
  • 2 replies
  • 1 kudos

Issues Communicating with MLX90393

I'm currently using a STM32 Nucleo-G071RB, I am trying to connect to a DAC (MCP4725) and also to a MLX90393 both using I2C, the DAC is connecting fine, but I am getting nothing from the MLX90393, has anyone used this device and been able to get anyth...

JNava.3 by Associate
  • 1291 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G0B1CET6 vs STM32G0B1CET6N

Hi everyone,I am not sure what is the difference between GP and N version of the chip. What I can find in the datasheet is that N version has additional VDDIO2 and VSS pins. If that is the only difference, what changes do these pins bring?Thanks! 

zoranr by Associate II
  • 3106 Views
  • 2 replies
  • 1 kudos