cancel
Showing results for 
Search instead for 
Did you mean: 

Value of register VTOR at reset on STM32H753

Gpeti
Senior II

The value of register VTOR at reset is "unknown" in the STM32H753 Programming Manual.

I assume this is because it depends on the boot configuration of the product (boot pin and boot adress option byte) ?

Is it correct to say that in the default boot configuration the value of VTOR at reset is 0x0800 0000 ? (I don't have a board to test it in the following days)

Also, when the VTOR is modified by the software, does its value go back to default for any kind of reset ? (warm reset, power on, etc...)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

The VTOR is initialized in the same manner on F7 series, which doesn't have the RSS feature. Most likely it's done by the same boot logic, which makes decisions based on BOOT0, option bytes, checks for empty flash on some series etc.

View solution in original post

3 REPLIES 3
Piranha
Chief II

RM0433 Rev 7:

  • 2.6 Boot configuration
  • Table 21. Option byte organization
  • 4.4.7 Description of boot address option bytes
  • 4.9.17 FLASH register boot address FLASH_BOOT_CURR)
  • 4.9.18 FLASH register boot address FLASH_BOOT_PRGR)

And, of course, the VTOR register gets back to one of those defaults on any kind of reset.

Pavel A.
Super User

From a short test on my Nucleo-H743, the reset value of VTOR is 0x080000000.

Not sure, however, is this the property of its CM7 core or effect of low-level ST firmware that decodes the option bytes and initializes the MCU (so called "Root Secure Service" or whatever).

The VTOR is initialized in the same manner on F7 series, which doesn't have the RSS feature. Most likely it's done by the same boot logic, which makes decisions based on BOOT0, option bytes, checks for empty flash on some series etc.