User Activity

Hello ST Community​I encountered many problems when using DFSDM peripherals,Especially the trigger problem of injection mode​The STM32Cube H7 package which providing DFSDM example,Only refer a applicableation About Audio​Can the ST official provide t...
When I use DFSDM, I configure FOSR= 256 ISOR=1 and the output is outside the range in the reference guide +-16777216
About EVSTSPIN32G4, I started the code generated by MotorControl Workbench 5. Y.3 normally.If you transplant the IIC configuration of the pre drive and enable PWM output, the VDS will report an error.After carefully reading the generated code, it is ...