STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L562CE 48-pin 1.8V USB

Hello,As I understand from datasheet if you use 64, 81, 100, 132 or 144 pin package there is separated power supply domain for USB transceivers, i.e. VDDUSB which should be connected between 3.0-3.6V or connected to VDD if USB is not used.However, 48...

STM32F769i-Disco

Hi, i'm trying to test the Eval STM32F769i-Disco with the B-LCDAD-HDMI1 Adapter.Is there anywhere a running Software to test this Hardware?Thanks DT24

DT24 by Associate
  • 1438 Views
  • 2 replies
  • 0 kudos

STM32H747 Audio Recording

Hey folks, I am writing to seek guidance as a newcomer to the MCU (Microcontroller Unit) realm. My objective is to facilitate audio recording utilizing the STM32H747 microcontroller. I kindly request assistance in steering me towards the appropriate ...

STM32 to LCD(8-bit CMSIS) help

Hi all,I need help. I am using the STM32-F446RE Nucleo-board and I have it connected to a 1602A LCD display. I am trying to write "Embedded" on the first row and "Systems" on the second row, but I get it all in row 1. Can someone look over my code an...

LCD Picture.jpg
HectorV by Associate II
  • 2327 Views
  • 2 replies
  • 0 kudos

Resolved! Use variables values from main.c in another file

if i use static UART_HandleTypeDef huart8; in main.c . when i want to run it in fpvisionai.c  HAL_UART_Transmit(&huart8,etc) say huart8 undeclared , should i use include <main.h> in this file,o how to set UART_HandleTypeDef huart8 as global variable

wjian.2 by Associate III
  • 3806 Views
  • 4 replies
  • 0 kudos

stm32h747-Disco uart8 sending trouble

I'm use uart8 to send data to arduino, but arduino no receive nothing, all the program is right complier,and the D1/D0 should be right(only have uart8).https://community.st.com/t5/stm32-mcu-products/stm32h747i-disco-virtual-com-via-usart-to-arduino/m...

wjian2_1-1692022116594.png wjian2_0-1692021766457.jpeg
wjian.2 by Associate III
  • 6595 Views
  • 17 replies
  • 5 kudos

Resolved! Question about SPI2 using PC_2 and PC_3

My project (Stm32H753) has 2 identical external ADCs, one on SPI2 and one on SPI3. The one on SPI3 is working fine, but I am having problems with SPI2. The code for them are the same, except of course different 'hspi' and pin assignments.The SPI is c...

XLin.2 by Associate II
  • 2455 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with 24LC64 EEPROM

Hi,I have a problem with an 24LC64 EEPROM, it is not a bad chip because i have tried 2 on diffrent boards. I am using the STM32G0B0  This are my I2C settings:I am using this libary : https://github.com/nimaltd/ee24/blob/master/ee24.cI only get 255 ba...

PieterInHetBos_0-1692625048920.png