2023-04-11 1:15 AM
2023-04-11 1:53 AM
Hello @LOnGr.1 ,
DMA1_Stream6_IRQHandler() is an interrupt handler for DMA1 stream 6.It adds a process to clear the transmit completion flag if it is present.
If the flag is not cleared, the next transmission will not be performed.
void DMA1_Stream6_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream6_IRQn 0 */
if( LL_DMA_IsActiveFlag_TC6(DMA1) == 1){
LL_DMA_ClearFlag_TC6(DMA1);
}
/* USER CODE END DMA1_Stream6_IRQn 0 */
/* USER CODE BEGIN DMA1_Stream6_IRQn 1 */ /* USER CODE
/* USER CODE END DMA1_Stream6_IRQn 1 */ /* USER CODE
}Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-11 1:53 AM
Hello @LOnGr.1 ,
DMA1_Stream6_IRQHandler() is an interrupt handler for DMA1 stream 6.It adds a process to clear the transmit completion flag if it is present.
If the flag is not cleared, the next transmission will not be performed.
void DMA1_Stream6_IRQHandler(void)
{
/* USER CODE BEGIN DMA1_Stream6_IRQn 0 */
if( LL_DMA_IsActiveFlag_TC6(DMA1) == 1){
LL_DMA_ClearFlag_TC6(DMA1);
}
/* USER CODE END DMA1_Stream6_IRQn 0 */
/* USER CODE BEGIN DMA1_Stream6_IRQn 1 */ /* USER CODE
/* USER CODE END DMA1_Stream6_IRQn 1 */ /* USER CODE
}Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-11 1:53 AM
Hello @LOnGr.1 ,
This works perfectly when using the HAL-function HAL_UART_Transmit_DMA().
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-04-11 1:54 AM
Yes, I already used the HAL function before, here I am trying to do it with LL
2023-04-11 2:08 AM
Hi! Thank you for replying. I am not able to find the function to enable the DMA transfer complete interrupt in the UM (I assume that I have to enbale it).
2023-04-11 2:23 AM
Here is it
LL_DMA_EnableIT_TC(DMA_TypeDef *DMAx, uint32_t Stream)
2023-04-11 2:45 AM
you can find this function inside : stm32fxx_it.c
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.