User Activity

We are continuing having a bear of a time getting the USB2514 to work properly with the STM327H73 both with the USB2514 built into our board and also with the STM327H73 connected to a EVB-USB2514BCQFM36 eval board.The latest issue is as follows:Conne...
Here comes another query about the status of a HUB device for the USB Host library. I have been working with the driver from herehttps://github.com/moribr/STM32F4HUB/blob/master/Project/Middlewares/ST/STM32_USB_Host_Library/Class/HUB/usbh_hub.cand ha...
We are having a bear of a time getting the USB2514 to work properly with the STM327H73 both with the USB2514 built into our board and also with the STM327H73 connected to a EVB-USB2514BCQFM36 eval board. Looking for suggestions for resolving this iss...
Having difficulty gaining access a peripheral region in the bootloader and could use some suggestions.In the bootloader we need to MAP the address space described below, this address space works correctly in the application but not in the bootloader....
Need to memory map the framebuffer in the bootloader, this is done using bspMpuConfig. when this is done the framebuffer can successfully be written but when transitioning into the next state the routine  /* RCC access done to identify the wakeup sou...
Kudos from