STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

G.722 vocoder

Hello,I've seen the AN4229-how-to-implement-a-vocoder-solution note, which talks about support for G.711 and G.726. Does anyone know if anything is available specifically for G.722?Thanks

EC.3 by Associate III
  • 1098 Views
  • 0 replies
  • 0 kudos

How to index different GPIO ports in one array

hi everyone.I'm trying to index different GPIO ports and pins.  #define STEP1_HALF1_PORT GPIOA#define STEP2_HALF1_PORT GPIOB#define STEP3_HALF1_PORT GPIOA#define STEP4_HALF1_PORT GPIOC#define STEP5_HALF1_PORT GPIOBGPIO_TypeDef *Half1StepPortNum[5] = ...

Resolved! Micro Trace Buffer (MTB) on STM32U5 devices?

Dear STM CommunityIn order to ease our debugging, I would like to make use of the Micro Trace Buffer which seems to be integrated in the Cortex M33 Core (e.g. stated by STM here: https://www.st.com/content/st_com/en/arm-32-bit-microcontrollers/arm-co...

Stef2 by Associate III
  • 2026 Views
  • 1 replies
  • 0 kudos

Resolved! iwdg is not working while usb device is running.

Hi,My MCU us stm32f401rct6.This MCU has three UART and all UART are using for service. No console UART port :(So, I make a USB CDC device to use console port.But, iwdg is not working. When I use UART console port, while(1); occur watchdog reset. But,...

Paul.Lee by Associate III
  • 3328 Views
  • 6 replies
  • 0 kudos

SPI1 with DMA Overflow Issue

I have SPI1 setup as Receive Only Slave with DMA enabled.  I send 10 bytes from SPI2 ( to simulate a full duplex master uC )  and it works well the first time I transmit 10 bytes.  When I transmit 10 bytes a second time, SPI1's overflow flag gets set...

LMorr.3 by Senior II
  • 2360 Views
  • 5 replies
  • 0 kudos

Resolved! Understanding MPU config for FMC LCD on STM32H7

Hi,I'm currently trying to understand the recommended MPU config (when settings up an 8 bit LCD connected via the FMC on an STM32H742. Everything is currently working, but I haven't been able to wrap my head around why configuring the MPU regions wit...

BEvan.2 by Associate II
  • 6895 Views
  • 2 replies
  • 3 kudos

Resolved! Wondering different port GPIO Power Consumption matter?

Hi everyone.I am recently working on stm32 chip and found a page show the power consumptionseems GPIO port C and F can save half the power than A and Bshould i always consider to use gpio port C and F ?or the consumption is too little that we don't n...

uveuvenouve_0-1692700092392.png

Copyright notice in main.c generated by Cube.

Posted on October 11, 2016 at 08:27Since the programmers are supposed to munge main.c into their own project, Cube generated code being just a starting point, why would ST put in a copyright notice that takes ownership of the code?This is the transi...

Strange behaviour when reading flash in FreeRTOS environment

Dear communityI have a strange behaviour, when I want to read the flash of an STM32U5A9 in a FreeRTOS task. I have a function, that programs incrementing numbers on a whole flash page of 8 KB (confirmed with J-Mem, that programming worked). If I want...

3839eb39-2548-42c2-af6c-bcf7a1d298ed.jpg
JWill.11 by Associate II
  • 2548 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L562CE 48-pin 1.8V USB

Hello,As I understand from datasheet if you use 64, 81, 100, 132 or 144 pin package there is separated power supply domain for USB transceivers, i.e. VDDUSB which should be connected between 3.0-3.6V or connected to VDD if USB is not used.However, 48...