STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! serial.peek() and serial.flush() equivalent in STM32

I'm trying to port a UART driver from aurdino to STM32. Able to relate all interfaces for aurdino vs STM32 while can't able to map ones for the followingserial.peek()serial.flush()Does HAL have an direct interface as peek() to get the next byte of in...

darthana by Associate
  • 7392 Views
  • 5 replies
  • 1 kudos

TICK_INT_PRIORITY changes from 0 to 15 and vice-versa

STM32CubeIDE - Version: 2.0.200.202301271415STM32CubeMX - Version: 6.8.1-RC4  Build: 20230419-1431 (UTC)I just added two DMA channels to UART1 and noticed a change in stm32h7xx_hal_conf.h The project uses LwIP and FreeRTOS. FreeRTOS relies on TIM6 as...

PriorityChanged.png
ARaid.1 by Associate III
  • 6049 Views
  • 6 replies
  • 0 kudos

I2C sensor on USART 2 Serial communication

Hello, I am using the embedded coder support package in simulink to interface with my onboard MEMS acceleration sensor (LSM303AGR) on my STM32F411VET discovery board. I could successfully connect and run simple LED program through USART2 on simulink ...

Resolved! Schematic of NUCLEO Board missing

Hi, I have bought a NUCLEO-F756ZG board to explore the F7 controller.I need the schematic to work with it. In the manual:https://www.st.com/resource/en/user_manual/um1974-stm32-nucleo144-boards-mb1137-stmicroelectronics.pdfThere is only a note on pag...

Moritz1 by Associate III
  • 3844 Views
  • 3 replies
  • 0 kudos

Resolved! ADC Sample Rate

I am doing current control with PWM. The switch provides a current sense pin which is going to my ADC.I am using STM32F4. I am also using FreeRTOS, not sure if this is important though.My ADC is set to run at 84MHz with 4x prescaler. The conversion i...

TonyFauci by Associate II
  • 4497 Views
  • 5 replies
  • 0 kudos

Facing issues with interrupts

Hi,I face some issue with the interrupts of STM32L452RET6P. I have two codes running in the controller one is a custom bootloader code and other is an application code which stored in flash memory. when the device get reset it will run the custom boo...

SSaiy.1 by Associate III
  • 3163 Views
  • 5 replies
  • 1 kudos

Library FingerPrinter for STM32 blue pill

HELLOI need to use a biometric sensor with stm32 blue pill (stm32f103c8t6) and I am looking for a library to use with the CubeIde software, does anyone have libraries for it?Thanks

robert456 by Associate II
  • 3640 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H757 Ethernet communication not working

Hello ST TeamI am working on medical project involving patient monitoringCurrently we are using the STM32H757XI-EVAL board and trying communicate the host monitor via ethernet TCP/UDP. The underlying operating system is Azure RTOS.I am not able to fi...

Lokesh1 by Associate II
  • 3794 Views
  • 4 replies
  • 0 kudos

Resolved! How to edit RTC Alarm parameters

Hi, I use RTC alarm to wake up from STOP mode I have STM32F030C8T6. During initialization I have set 5s and everything works as it should. But I would need to change the interval to maybe 30s while the program is running. The problem is that the chan...

DJeze.1 by Associate II
  • 9700 Views
  • 2 replies
  • 0 kudos