2023-05-10 7:59 AM
hello,
Which command is valid to do this? I see --skipErase, I have also seen --ske, or ske as possible commands to use.
What is the syntax for this command? I dont see a reference in the manual...
Please help thanks in advance.
2023-05-10 9:19 AM
Hello @RobNeWin ,
The equivalent of 'Skip Flash Erase' option is 'ske' to be used with ST-LINK_CLI.exe.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-10 9:36 AM
@KHALSI_Foued great, what is the syntax to send this command?
Do I do this before the download (-w)? or after? or a separate command?
thanks!