STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

low power measurement for nucleo L073RZ with stlink-v3pwr

Hello I just brought the stlink-v3pwr. I also have the nucleo L073rz. I want measure the current consumption. To do that I wrote a simple example by calculating the float values multiple times and then provide 1 sec delay. I supply power to the nucle...

ABans.3 by Associate II
  • 1430 Views
  • 0 replies
  • 0 kudos

STM32G0B1KxT CAN not working

Hi Team,I am using STM32G0B1KxT and code is successfully uploaded. The code is referred from sample code only still it is not working. Here CAN is CANFD but I am using as classic mode.I am attaching snippet of CAN part and main.c file.    

CAN.PNG

STM32WB5MMG BLE problem

I make a board using STM32WB5MMG. The I2C and SPI communications are normal, but I find a lot of problems about BLE function.After using BLE p2p server.ioc (based on stm32wb5mmg) to generate the IDE project, the Bluetooth broadcast cannot be found an...

Lep by Senior
  • 2903 Views
  • 3 replies
  • 0 kudos

RTC stm32f103

Hi. I need help with RTC on STM32F103. I would like to edit the time (hours and minutes) in my RTC using a button. When I add an hour the maximum vartosc I can reach in the RTC->CNTL register is 65535 (18h20min), when this value is exceeded, the regi...

Resolved! How to convert .elf file to stldr manualy(without a command)?

Hi, i want to convert my generated .elf file to .stldr file. I need a stldr file for CubeMX programmer, so that i can use it to program my external flash memory(write,erase, read). I have seen in the video from ST about external loader, that the ST-e...

FLuba.1 by Senior
  • 3308 Views
  • 3 replies
  • 2 kudos

related to high end video processing

Hi community, did anyone use 8MP USB camera like imx179 or above versions ,using this stm32H7 series, i wanted to make a drone using this , if anyone has made please share , and also what specification camera are available for this stm32H7 series . 

amam by Associate
  • 4401 Views
  • 0 replies
  • 0 kudos

STM32F407IG Ethernet (UDP)

Is there an example or link where I can see the code for STM32F407IG Ethernet (UDP) communication?https://www.st.com/en/embedded-software/stm32cubef4.htmlThe link here doesn't have the code I want- UPD Ethernet connection- Code for Ethernet Receive a...

STM32U575 timer triggered DMA for autonomous SPI transfers

Hi,I have a STM32U575 connected to an external HW watchdog which needs to be periodically fed (with a 100 ms timeout) with an SPI command from the MCU (2 bytes), and i would like to achieve this without CPU intervention (or as little as possible).Her...

image.png
SBone.3 by Associate II
  • 5848 Views
  • 2 replies
  • 0 kudos