Hi ST experts,I am using the AT command code from ST on the B-L072Z-LRWAN1. I have loaded the bin into the B-L072Z-LRWAN1 via ST-LINK3 switch on the RS232 @ 9600 and get the terminal screen with the AT command working very well. I have a KERLINK gate...
Hi ST experts, Can help to advise that 9axis (IMU+Mag) is a viable solution for indoor head tracking and positioning?There are multiple references stating that the magnetometer is prone to magnetic field interreference indoor and is suggested to ign...
Hi ST experts,Does STM32G4 series MCU support Vocoder feature? If yes, do you have any related documents available for reference? Current design is using STM32F405 which can support Vocoder application. Thanks.
@JTuckerBCA Hi, One more small issue to cross before production. I cannot get the Fcnt (Frame count) to be incremental of +1 but rather +256 when using the thingpark with ABP mode. OTAA you mentioned add 5000ms on the link and it worked like a charm....
Hi @STOne-32 ,Yes please, I can share the project details in the email. Do help to share the report asap as we need to review it urgently. Appreciate your help.