STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030CC Custom PCB - STLINK V2 Programming Issue

Hello STM32 communityI'm facing an issue with my custom PCB featuring the STM32F030CC microcontroller. I've been using an STLINK V2 with opto-isolation for programming via SWD.Here's the scenario:Initial Success: After connecting power and performing...

Jouls by Associate II
  • 4455 Views
  • 7 replies
  • 1 kudos

Questions to functional safety according 61508 (SIL 3)

Hi together,I have some questions depending to the qualification proccess. It is planed to use STM32L451, there is an IWDG which is, as the name tells independent, so can I assume that I can do the project without an external watchdog device, if we u...

PCB design guidlines for STM32WB5MM module

hi,In the page 13 of the datasheet (https://www.st.com/resource/en/datasheet/stm32wb5mmg.pdf) there is limited information about the PCB layout guidlines. I'd like to know more about the layout on left side of the module in the image shown if the mod...

Vansh_0-1693790409011.png
Vansh by Associate II
  • 7925 Views
  • 7 replies
  • 1 kudos

STM32F107 reset failed via NRST pin

Posted on October 20, 2016 at 05:54Background:       1.5% of products which use STM32F107 totally dead after using 3 months;Problem:       The NRST reset not function. After disconnecting the power and connecting again, the chip could recover and wo...

0690X000006058PQAQ.png

Problems with CDC and FreeRTOS streams

I'm experiencing a weird race condition / hangup with an application that I've built for my STM32F407VGTx. Basically I connect to the device via a USB cable and open a terminal to type commands on the device like a CLI. Everything works fine until I ...

Screenshot 2023-09-14 at 8.21.27 PM.png
bdill.1 by Associate II
  • 1416 Views
  • 0 replies
  • 0 kudos

STM32U575 - USBPD_CAD_Init error wit Thread-Safe setting

Hello,I am building an application using ThreadX, FileX, USBX and USBPD. Everyting runs perfectly until I bring USBPD in the game. Whatever I do, I always get an error when the library calls USBPD_CAD_Init().More precisely, the function fails at a ca...

Pepils by Associate II
  • 4208 Views
  • 5 replies
  • 0 kudos

Regarding STSW-IMG010

Hi, I have  X-NUCLEO-53L0A1 and X-NUCLEO-53L5A1 board can any of these boards be used to run the STSW-IMG010. The documentation in STSW-IMG010 mentions that we should use a X-NUCLEO-53L1A1. Please let me know if I should make any modifications to mak...