STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hardware timer interrupt Delay in STM32G4

Hi,I am working with STM32G4. I am generating 1Khz PWM from my Timer2 and TImer1 I am using for delay(I configured it for 50 usec delay with interrupt).Both timer2 and timer1 working as expected.1.For every pwm pulse start I need to read adc for 50 u...

Resolved! Having Issues with ADC configuration STM32L011K4T6

Hello,  I have tried for the last couple of days to get use 2 pots to change the frequency and duty cycle of a PWM signal using "Bare Metal" programming due to the flash limitation of the STM32L011K4T6 I rapidly ran out of space using HAL and was not...

Triggering SPI DMA transfer with TIM1 event.

Hi everyone,I am using STM32F410 CPU.I need to send 4096 bytes of data via SPI using DMA transfer.The transfer should be triggered by each TIM1 event.I have read these two posts:https://community.st.com/t5/stm32cubemx-mcus/trigger-spi-dma-transfer-fr...

load2005 by Associate III
  • 2550 Views
  • 3 replies
  • 0 kudos

Elf loader is bigger than RAM size

Hello I am using STM32L010k4 controller for one of my project. And I am trying to program using stlink utility. My binary file size is 7.5kb. - my controller is successfully connected from utility- I can successfully erase chip by stlink utility But ...

Resolved! I was Unable to use RTR(Remote Transmission Request) in CAN using STM32F407VGT6 and STM32F302R8

I tried to send a RTR frame to another CAN peripheral , another node received the RTR bit successfully and RTR bit in the node has been set. Does the node receiving the RTR frame will transmit the Message automatically? or We have to read the RTR bit...

CAN question with STM32F103C8T6.

Hi all!,I have 2 STM32F103C8T6 connected by CAN bus.Each STM32F103C8T6 has the same firmware.This firmware starts sending a message "RequestID" by the CAN bus.Is there a way to avoid send the "RequestID" in case another "RequestID" were detected on t...

JAlca_0-1699692973609.png JAlca_1-1699693190500.png
JAlca by Senior
  • 1426 Views
  • 1 replies
  • 0 kudos

Resolved! Issues with CANBUS on STM32F072: Bit Dominant Error

Hello,I am currently working to get CAN transmission to work on a STM32F072B-DISCO. I am continuously getting a BIT_DOMINANT_ERROR in the LEC of the CAN_ESR when attempting to transmit. I am using a TCAN1044 (https://www.ti.com/lit/ds/symlink/tcan104...

PF-JohnF by Associate
  • 4712 Views
  • 4 replies
  • 0 kudos