STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lost debug messages from LORA WAM STM32WL device

I lost debug messages from my LoraWAN end device. I made some changes using MX on my project, and this way, I lost debug messages displayed on a serial wire monitor (for example, on Arduino serial monitor). I think it was the cause of this problem. N...

markpow_0-1703241149646.png
markpow by Senior
  • 3811 Views
  • 10 replies
  • 0 kudos

Resolved! STM32 with capsense support and ethernet available?

I've taken a look at AN5105 (Getting started with touch sensing control on STM32 microcontrollers) where they present a list with microcontrollers that support capsense:STM32F0 seriesSTM32F3 seriesSTM32L0 seriesSTM32L1 seriesSTM32L4 seriesSTM32L4+ se...

petervg by Associate
  • 2490 Views
  • 2 replies
  • 0 kudos

STM32F401RET6 RTC initialization failed one power up

Hi,The RTC block was driven by LSI (internal RC osillator), we just found few boards failed to initialize the RTC block and the program was stuck there. What could be the possible reason? Is it due to the floating pin of Tamper?thanks,Qi

QiWang by Associate
  • 1149 Views
  • 1 replies
  • 0 kudos

STM32F401RET6 failed UART communication

We just found few boards failed UART communication. The debug process for this issue points to the LSI and RTC block inside the MCU STM32F401RET6. The RTC block was driven by LSI (internal RC oscillator), these boards failed to initialize the RTC blo...

NealXu by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F407 CAN Loopback Mode work but Normal Mode not working

Hello, I am trying to establish standard CAN communication between the sn65hvd230 IC and the stm32f4 discovery and stm32f103. While the loopback mode works fine, when it sends data to the normal mode, the output goes to 0 and then back to 1. I still ...

Sergen by Associate III
  • 10598 Views
  • 11 replies
  • 0 kudos

STM32L432 Nucleo board: ADC has -53 mV input offset ?

I'm using a STM32L432KC Nucleo board, and reading a voltage with the 12-bit ADC. On this board the ADC Vref is connected to the board 3.3V, which in this case actually measures 3.315 V.  With a 12-bit resolution, I would expect that 4095 ADC counts =...

JBeal.1 by Associate II
  • 2538 Views
  • 4 replies
  • 0 kudos

STM32L073 datasheet incomplete information

Hi,As per DS10685 Rev 7 (https://www.st.com/resource/en/datasheet/stm32l073v8.pdf), there are so much information missing, for example:1. Table 17 doesn't mention that the USB pins D+ and D- are bound to PA11 and PA12 ports, respectively, but Table 1...

XR.1 by Senior
  • 1572 Views
  • 2 replies
  • 1 kudos

Resolved! STM32L476 SPI3 Using DMA2 Chan 2. No Transmit.

Hello Everyone. My how the forum has changed. Just dropping a recent odd experience here to see if anyone might have any comments. No. I don't use CubeMx and no this isn't another 3 year anniversary item regarding initializing the DMA before any peri...

Octospi vs FMC

Hi,I am doing a new design of a board and I am wondering what is better to have as in interface for a external memory FMC or Octospi? Thank you

aabba.1 by Associate III
  • 4717 Views
  • 2 replies
  • 2 kudos