I couldn't understand the pinout of the nucleo boardHere in CN8 the blue side pins is mentioned with both D43 and PC8. same in CN7 pin number 1 is mentioned with both PC6 and D16. But which of pin is actually connected to this specific header.
Hii thereI am using STM32F410RB (M4). it has a flash of 128 KB divided into following 4 sectorsMy query is that I want to store and retain some non-volatile data in the flash. We can use the last few pages of the flash for this purpose. I have come ...
I was wondering if I could find any library for simulating IR signals with an STM32 microcontroller. I couldn't find any library for this purpose. While I did come across some work done by Controllers Tech on receiving IR signals from a re...
Hii everyone,i am working with a 2.8 inch spi display, using ili9341 display driver, adn it is having xt2046 touch driver on it.Can anyone please guide me for the right and stable library available for using xt2046..i am unable to find any
Thanks for the reply TDKI have few more queries regarding the same, as per your statement mentioned above "a flash sector and a flash page are effectively the same. You can't erase less than an entire sector" we can't erase less than a sector or a pa...
HiThanks for your response,As much as i read at the website it only supports RC5 protocol &SIRC protocol. I was looking for the implementation of NEC which is an standard protocol. Is it possible to do so?