I am looking for a development board, but have multiple requirements, so I will order them here, to help you answer me, plus to help me to order my own thoughts:- Grove connector support, preferably on-board, otherwise with a clip on shield (...
Hello,I have done with flash via dual boot option on a STM32L476RG board using an external board NUCLEO- L476. when I am trying to change the option bit via program in which i am using HAL_FLASHEx_OBGetConfig and HAL_FLASHEx_OBProgram. eventually i a...
On the storage device on the nucleo-h743zi i just bought is a file "MBED.HTM"the ARM page https://os.mbed.com/platforms/ST-Nucleo-H743ZI/ explains:WarningThis platform is not yet available on mbed on-line compiler. Please use mbed-cli commands in the...
Hi,For our application we want to write a region in flash with configuration files during production. This is handled by the Segger JLink that writes the program bin and the configuration bin in two parts of the memory.While the firmware can read out...
I am using STM32F769 Disc board with Mbed online compiler. My task is to change the PWM frequency and duty ratio according to input. i created a simple algorithm according to my need, the program is working well but whenever the controller updates th...
Hi STM32,I'm using STM32F401RE for communication with PC and want to send packet at 3-5 MBps speed.I have to use MBED OS for deveopment kindly support for this also on my board 3x cryastal is not mounted only 2x so also want to conform my controller ...
I'm using Mbed online compiler to program the micro-controller, i have i2c library in mbed compiler, and also have 24C08 External EEPROM IC, if required.
Posted on May 12, 2017 at 12:49Hi,seems that I'm having many problems using the peripherals I need for my MSc Thesis project with the Nucleo-L432KC.Now it's time to have problems with the microSD card module.I bought this module:https://www.amazon.i...
Does anyone know when stm32H743zi and Nucleo-h473zi will be aviable on os.arm.Mbed platform?