STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H5 Need bootloader pins

As per errors in AN2606 and this thread https://community.st.com/t5/stm32-mcus-products/stm32h5-bootloader-uses-usart-pins-that-do-not-match-roles-in/m-p/594610#M224078 I need the correct pins that STM32H563/STM32H573 use for USART1/2/3 and FD-CAN bo...

MBC by Associate III
  • 797 Views
  • 6 replies
  • 3 kudos

Resolved! Typos in AN2606

 Pages 249 and 254Also, the flowchart on 254 does not show USART anywhere. 

MBC_0-1696546180188.png
MBC by Associate III
  • 594 Views
  • 4 replies
  • 1 kudos

application note and data sheets

In the installed STM32Cube Repository there are hundreds of application notes and data sheets, does anybody know where there is a list of contents?  It would take a long time to open them all to check or get the right grep phrase to search.

billium by Associate
  • 90 Views
  • 2 replies
  • 0 kudos

Resolved! AN2606 missing STM32G4A1 series

I'm trying to configure the Bootloader for a STM32G4A1KE processor, but in the AN2606  I cannot find any information regarding this processor (family STM32G41). Although it is listed in the introduction section of AN2606, no further information is gi...

Example script/program for I2C bootloader commands

Hi, I'm using a STM32G07x1 that will need to receive firmware updates from an embedded Linux CPU. The only connection between these devices is an I2C bus so I plan to use the ROM I2C bootloader to handle updates.I am aware of AN4221 that describes ho...

Resolved! STM32C031 pin PF3

Hi, I was reading the document "DS13867 Rev 3" (datasheet for STM32C031x4/x6) (https://www.st.com/resource/en/datasheet/stm32c031c6.pdf), and while searching about pin PF3, I found this strange information saying that it is a "Supply" pin type. I've ...

Hagi_0-1698686217782.png
Hagi by Associate II
  • 90 Views
  • 1 replies
  • 1 kudos

Flash wait states meaning

Hi i have a generic doubt about falsh wait states:Say we configured the PLL to run system core clock at 160 M Hz, with flash wait states as 5.Then is cpu is equvilent to 32 MHZ core performance? (assuming 1 clk/ 1 inst, no ART's)Could some one help m...

RKall.1 by Associate II
  • 108 Views
  • 2 replies
  • 0 kudos