User Activity

RM0444 (Rev. 5 Nov 2020 - should be newest): Chapter 15.8 Oversampler: "N is defined using the OVFS[2:0] bits": this should say "OVSR[2:0]" bits. Chapter 15.12.3: Register ADC_CR Note for AD_EN: "set ADEN only when all bits of ADC_CR registers are 0"...
Hello,I would like to use TWO circular DMA buffers for ONE I2C interface.Depending on received address byte, in the ADDR interrupt I would always enable the correct circular buffer (disabling the other one - so at one time always only ONE buffer is a...
Hi,in RM STM32G4 (I use Rev. 7, page 1882, Figure 648 "Transfer sequence flow for I2C master transmitter for N>255bytes":The "RELOAD=0" info in last box at "N<256" is wrong.It must instead say RELOAD=1, AUTOEND=1 (otherwise Stop bit will fire immedia...
Hello, I would love to add a USB storage device (USB stick) to my terrific new STM32G4 application.But I am frightened, with the STM32G4 USB device interface this is impossible?(or this there some way to come around this?)(or is there any possibility...
Hi,I want that my user can re-program (through my application) some upper part of flash for configuration of the device, e. g. the upper 100 kByte.Until now, I used STM32G473, there this was no problem, as this was dual-bank memory device.Now I would...
Kudos from