STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Boot Library

I'm using an STM32H745 and have developed the Boot code, which works as expected when built as part of an application.  However, having converted the Boot code to a static library and linked it into the same application the Boot startup section .isr_...

NBrick67 by Associate II
  • 1724 Views
  • 2 replies
  • 1 kudos

Can't erase/write some Flash page in STM32G071RB

Hello,I'm writing a Flash HAL driver in order to understand better how this CHIP work.My functions at the moment work correctly but for some page I have an HardFault(During erase).For example I can't erase/write the page 0 and others pages.Please cou...

dmrsim by Associate III
  • 2286 Views
  • 3 replies
  • 1 kudos

HID issue with multiple report id

Hi Everyone,I am currently using STM32F103 for making a usb hid which acts as both, a keyboard and a gamepad.Please take a look at the descriptor and code below.Both of these work properly when used individually but when I combine them both and add r...

aksh3101 by Associate
  • 4655 Views
  • 3 replies
  • 0 kudos

ExT interrupt not firing.

we are using EXTI1 interrupt in our project based on stm32f446. But the Interrupt handler is not firing.We looked into the interrupt enable registers, Mask registers, etc and all seems fine and a timer interrupt also in the project, which is triggeri...

KumarTP by Associate III
  • 3637 Views
  • 4 replies
  • 4 kudos

Resolved! Avoid cross-effects between the LC sensors

Hi all,I'm using application note AN4636 for LC sensor.I tested with the example source code, and they work well for one sensor.But when I use multiple sensors, I face an issue. If I use the same value for inductor and capacitor for each sensor, the ...

phoungvd by Associate II
  • 4579 Views
  • 4 replies
  • 2 kudos

Resolved! stlink v3 mini cannot program c031g4u6, Target no device found

i am sorry for creating a lot of post recently but i just can not program my microcontrollers. when ever i try to program it i get this:STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rights reserved. S...

WhatsApp Image 2024-01-11 at 22.24.12.jpeg WhatsApp Image 2024-01-11 at 21.59.11 (3).jpeg WhatsApp Image 2024-01-11 at 21.59.11 (2).jpeg WhatsApp Image 2024-01-11 at 21.59.11 (1).jpeg
oyalç.1 by Associate III
  • 8518 Views
  • 16 replies
  • 7 kudos

Single ADC Reading with Multiple DMA Channels

Hi,Is it possible to have a single ADC result transferred to two different memory locations using DMA without CPU intervention?Specifically I want DMA to take a single reading from an ADC, transfer it to one location on the STM32H747 CM4 and another ...

slc2015 by Associate II
  • 2127 Views
  • 3 replies
  • 0 kudos

STM32G491KCU6: Unable to program via UART1

Hello,I'm trying to program G491KCU6 board via UART1 and I'm not able to connect to st-programmer. I don't know whether the board is actually entering Boot0 or not. I have PB8 with 10K to GND and I pull it up during connection to enter Boot0. Below i...

MallikarjunSE_0-1705136656649.png