cancel
Showing results for 
Search instead for 
Did you mean: 

RAMECC interrupt enable register (RAMECC_IER)

KevinG
Associate II

I am trying to test code which has been written to deal with RAMECC errors. The MPU is STM32H753 and I am working on a Nucleo-H753ZI board.

The first problem was how to simulate a RAMECC error. I found the code at https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/NUCLEO-H745ZI-Q/Examples/RAMECC/RAMECC_ErrorCount and I was able to copy the relevant code over to a new project and get it working.

However, I find that the sample code appears to disable all interrupts in RAMECC_IER at memory address 0x52009000 and never turns them back on. In spite of this interrupts do happen and produce sensible numbers in the status registers. However, I find that if interrupts are enabled in RAMECC_IER (specifically if bits 0, 1 or 2 are set) then while interrupts do still occur no sensible numbers are returned in the status registers.

RAMECC_IER set to zero, sensible numbers returned in status registers

working.jpg

RAMECC_IER set to F (all interrupts enabled), status registers are all zeros

notworking.jpg

What is going on here? Is the documentation wrong?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Issamos
Lead III

Hello @KevinG 

I think that the AN5342 may help you. 

Best regards.

II

Sorry but no it doesn't.

FBL
ST Employee

Hello @KevinG ,

I will check internally and get back to you.

Thanks

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL