STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I set the NUCLEO-L476 to Low power mode

I need to use the energy collection mode of ST25 to wake up L4. The software used now is En.X-Cub-NFC7. How can I modify the example code to set L4 to low power mode and wake up L4 only through the energy of ST25?

Resolved! Uart receiver pb

 i have established communication with a BLDC (Brushless DC) controller. Initially, i send a message to the controller using the function void sendParameter(uint8_t parameter). Following this transmission, the BLDC controller is expected to respond w...

kkhli.1 by Associate III
  • 21825 Views
  • 26 replies
  • 11 kudos

Resolved! NUCLEO-144 H723ZG "Can not connect to the target!"

Hi there,I received a new out of the box NUCLEO-144 H723ZG board which I can not connect, but getting the "Can not connect to the target!" message (see below)What I've done so far:- checked the Jumper as described in user manual UM2407 section 5 >> a...

PGrif.2 by Associate III
  • 3938 Views
  • 7 replies
  • 2 kudos

Resolved! NUCLEO F411RE, interrupt preemption priority is not available.

I am trying to set up a multichannel ADC and following YouTube tutorials to create it. However, the STM32 IDE will not allow me to set preemption priority to 1. Similarly, I cannot set the clock prescaler as divided by 2.  I need to make a multichann...

niru_0-1705330259946.png niru_1-1705330324783.png
niru by Associate
  • 2663 Views
  • 4 replies
  • 0 kudos

Resolved! Where are the schematics for NUCLEO-H743ZI2

Hello,I have here two Nucleos with an H743 on it. If it is rev Y, it is the "old" 144pin Nucleo board with the break-off ST-link board on top. For this there is a schematics in appendix A of the user manual. But if it is rev V, it is NUCLEO-H743ZI2 ,...

stm32 dma request synchronization settings

Hi,I have an external SPI 8 channel ADC which is connected to the STM32,one of timers would generate a 32KHz 50% pwm signal which is connected to the ADC convert pin, the ADC has a busy pin which is connected to the EXTI0 of the MCU.The plan is to us...

Screenshot 2024-01-14 165113.png Screenshot 2024-01-14 165135.png Screenshot 2024-01-14 165144.png Screenshot 2024-01-14 165120.png

Resolved! STM32H743 - ADC wrong sampling rate

Hi STM32-Community, I'm using an STM32H743 with ADC3 in circular DMA mode. ADC has a clockfrequency of 48 MHz. I'm using 8 channels within this ADC3 and also configured the DMA with said channels each with a sampling time of 64.5 cyles. I'm using an ...

NW2_0-1691752233265.png
NW.2 by Associate II
  • 3847 Views
  • 4 replies
  • 1 kudos

Unwanted flash erase issue

Hi, I am using STM32L072CZT6 for my project. The device operates in two stages: It wakes up at scheduled intervals, save the number of interrupts received to flash , and returns to standby mode. During standby, interrupts wake the device, the count i...

Deepu joy by Associate II
  • 2239 Views
  • 3 replies
  • 1 kudos