STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743 Save ADC Output from DMA to RAM to Flash

Hi all, im using Cube IDE STM32H743ZI2 Evaluation boardim curently sampling ADC2 and storing the output at an internal array using DMAthe array size is uint16_t[100,000]my requirements as to store much more data which means i have to use a diffrent m...

shahaf321_0-1707061080066.png
shahaf321 by Associate III
  • 3531 Views
  • 5 replies
  • 3 kudos

Resolved! Revert .ioc file for older CubeIde version

Hello,I recently upgraded to CubeIde 1.6.0 but I am having many new problems when programming STM32h/43: the configurations generation is much slower and it often stops updating all needed files, which forces me to reboot (I could not find a better w...

SSorr.1 by Associate II
  • 5753 Views
  • 4 replies
  • 1 kudos

STM32F439 Ethernet Frame Transmit Jitter

Hello,I have some questions regarding Ethernet frame transmission.1) When is the value of the "ETH_MMCTGFCR" register increased?After calling the "HAL_ETH_TransmitFrame()" function, I noticed that the value of the "ETH_MMCTGFCR" register increased in...

2024-01-31 181125.jpg

STM32 UART stops At High Temperature

Hi,I am Using an stm32f205 on our board. All the Uarts works fine at room temperature. But when the temp increases above 58 degress, messages started get missed in the uarts or sometimes it completely stops sending messages.I am running the board at ...

JThom.15 by Associate III
  • 5876 Views
  • 10 replies
  • 6 kudos

USB gadget

 I have successfully configured USB On-The-Go (OTG) on an STM32 microcontroller to support both Abstract Control Model (ACM) and Human Interface Device (HID) protocols. I utilized the stm32_usbotg_eth_config.sh script as a reference, and the setup is...

Barak1 by Associate
  • 1578 Views
  • 1 replies
  • 0 kudos

Resolved! Measuring elapsed time in nanoseconds

I need to measure the time it takes for a component to reach a certain voltage, read out with the ADC. So far I have been measuring in microseconds but it turned out that that is not precise enough.I found the following code to measure time on Stacko...

Qwyntex by Associate III
  • 17432 Views
  • 13 replies
  • 3 kudos

Needed help in ADC callback using Interrupts.

__IO volatile uint8_t ADC_ConversionFlg=0;void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc){/* Prevent unused argument(s) compilation warning *//*ADC_ConversionFlg |= 0x01;CTP=HAL_ADC_GetValue(&hadc1);} MX_ADC1_Init(); HAL_ADC_Start_IT(&hadc1); ...

Tushar_4 by Associate II
  • 2068 Views
  • 3 replies
  • 1 kudos