2023-10-18 8:13 PM - edited 2023-10-19 3:59 AM
Hello Developers,
In my product solution based on STM32L496VGTX, i am currently adding NFC DFU feature. Using the demo examples we were successfully able to receieve and store the firmware packets using mailbox of ST25DV04KC module. But after firmware validation whenever i call function to swap bank and reset the board, the new firmware is not getting loaded.
So i thought of testing Dual Bank swap for my selected controller i.e STM32L496VGTX. I have tried to implement the same issue in a standalone project which i have attached for your reference. Where demo binary example (Red led blinking f.w) is programmed at address 0x08080000 (bank 1) using STLink Utility.
Now using STM32Cube IDE i am running code on bank 0, with Blue led blinking. On button press the banks will swap and reset will take place. But for some reason i am unable to switch to new firmware.
So can anyone please look into this issue. I have attached the project file containing all the code needed for bank swap.
I have reffered the following links for refference:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.