STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Technical Updates are back : 2024 Newsletter 1 !

Dear STM32 users and developers, This new thread is back and is dedicated for our technical developers community to share last STM32 updates, the first part will be products documentation news such as datasheets, Erratas, Applications notes  followed...

STM32 Technical updates - 2024 Newsletter1.png
STOne-32 by ST Employee
  • 5669 Views
  • 8 replies
  • 16 kudos

Resolved! STM32H755 CM7 Reset_Handler Stuck at 'ldr sp, =_estack'

Hello everyone,I am currently working on a project using the STM32H755 microcontroller, and I am facing an issue with the program getting stuck in the `Reset_Handler` during debugging. Specifically, the code halts at the instruction `ldr sp, =_estack...

durna by Senior
  • 3961 Views
  • 11 replies
  • 0 kudos

Resolved! STM32L0 cannot change PWR_CR_ VOS

Hi, I'm stuck on a problem with setting PWR_CR_VOS on NUCLEO-32 STM32L031K6- I want to select HSI16-PLL as clock source- VDD is 3.3V- FLASH latency is set to 1WSBut I can only set PWR_CR_VOS to RANGE 2 and RANGE 3.RANGE 1 cannot be selected, so I can...

RinGO by Associate III
  • 1336 Views
  • 9 replies
  • 0 kudos

RTC LSE not working with VBAT on poweroff

I am working on an STM32 device with TrustZone enabled, and I am using the RTC with backup domain powered by VBAT. My RTC is initially configured while VDD is present, and after power-off, the time is supposed to be retained using VBAT.When I use the...

Ananth_ by Associate II
  • 481 Views
  • 2 replies
  • 1 kudos

Resolved! DBP bit couldn't be set to 1

I want to use stm32f103rct6 inner RTC, I write some code as below to active RTC, But I found I couldn't set DBP bit of PWR_CR reg to 1,   __HAL_RCC_PWR_CLK_ENABLE(); __HAL_RCC_BKP_CLK_ENABLE(); LL_PWR_EnableBkUpAccess();when I debug the re...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.