STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446 EXTI GPIO interrupt not triggering

Hello, I’m working with an STM32F446 and have configured GPIOB pin 12 as an EXTI input. After initialization and before entering the main while loop, I call a function that blocks program execution(what I mean by blocking : I have a test that stands ...

ISSUE with STM32L051C8T6

Dear ST Team,我用usb转ttl单独对4g模块发at,回复消息是正常的,单独模拟给单片机发数据,回应的数据也没有丢字符,就是4g模块跟单片机之间通信的时候存在问题When I use a USB-to-TTL adapter to send AT commands to the 4G module alone, the responses are normal. When I simulate sending data to the microcontroller alone, th...

Resolved! Crystal and Capacitor Select for STM32H743VIT6

Hello, I want to design a PCB with STM32H743VIT6 MCU. But I am not sure how can I choose crystal and capacitors properly. In STM32H743VIT6 datasheet there is one section about this topic;according to this information should I take the Cstray value as...

testbenchmark_0-1764852672590.png testbenchmark_1-1764852684709.png testbenchmark_2-1764853006389.png

Resolved! STM32F103 UART Bootlader: "Error activating device: KO"

Hello,I'm new to this STM32 products. We designed custom module with STM32F103CBT6TR. We are facing issue with serial boot loader.I'm using CH340 UART to USB converter module. CH340 MOD TX --> Our Module's RXCH340 MOD RX --> Our Module's TXCH340 MOD ...

gadi_0-1765184162415.jpeg gadi_1-1765184232337.png
gadi by Associate II
  • 1881 Views
  • 14 replies
  • 2 kudos

Resolved! STM32N6 I2C Logic Levels

I have an I2C device that only operates with 1.8V logic (Pins are not 3.3V tolerant) that I want to connect to the STM32N6.  I don't want to add an I2C redriver if I can avoid it.  I want to keep as many of my I/O pins on the STM32N6 powered from 3.3...

Lucky1 by Associate II
  • 642 Views
  • 4 replies
  • 0 kudos

Resolved! UART not working at High speed

Hello, I’m trying to transmit data at 2.5 Mbps (2500000 baud), but I’m not receiving any output. The same code works correctly at 2 Mbps, so the issue only appears when using 2.5 Mbps.I tested both 64 MHz and 40 MHz clock configurations for the UART....

Rohit007 by Associate III
  • 1325 Views
  • 13 replies
  • 8 kudos