STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L151 ADC

I am working with the above device. I have created an .IOC file and auto-generated code. I can see the GPIO configuration for the simple I/O, but I do not see any pin configuration for the ADC inputs that I have selected. I assume that I will have to...

Wyorin by Associate
  • 1492 Views
  • 1 replies
  • 0 kudos

CS42L52 CODEC Not Working On Keil MCBSTM32F400 board

Has anyone ever had success getting the CS42L52 audio CODEC to work on the MCBSTM32F400 board? It is suspicious that there are no working code examples for the CODEC and it is also left out of the board's BSP support package. I have taken the time to...

BarryB by Associate
  • 898 Views
  • 0 replies
  • 0 kudos

SMT32L4 power consumption to high

Hi all,I have a project with a SMT32L431. Right now it is running on the nucleo-64 demo board (its a STM32L4 33RCT6P) so nothing is connected to the board.The project will use all UART and LPUART modules, the SPI1, the I2C2 and the CAN1 module. I hav...

bareil76 by Associate II
  • 1626 Views
  • 2 replies
  • 1 kudos

Resolved! LTDC usage on stm32h735 to display an image of 40x80

Can anyone tell me a sample code for LTDC display where im using stm32h735 and using a particular image of         40 x80 and wanted to display on LTDC display. Is there any better way to learn how to code for LTDC   

sid1401w by Associate
  • 1731 Views
  • 1 replies
  • 2 kudos

Resolved! STM32H7A3 Unique Device ID number question

Hi @mƎALLEm,I need to develop a unique serial number for one of our products that will go into production soon. I'd rather use the UID that is built into the STM32H7A3 chip but I have some questions.I understand that it is a 96bit value that I can re...

Resolved! ST bootloader - pin states

Hi,I'm currently gaining experience with the STM32G4, whose ROM bootloader supports various interfaces. AN2606 describes the configuration of the pins occupied by the interfaces.Various pins are operated in push-pull mode, which can lead to undesirab...

kf_SEA by Associate II
  • 2404 Views
  • 3 replies
  • 0 kudos

Expereincing watchgog reset issue while machine is running.

Hello everyone,I'm currently working with the "STM32G0B1RE" and facing an issue where my system automatically resets. The problem occurs sporadically, sometimes after a week and other times within 2 or 3 hours. Upon investigating, I found that the la...

asth_raj by Associate
  • 1744 Views
  • 3 replies
  • 2 kudos

How to check ROM and RAM?

We are trying to add built-in self-test capability to a program we are developing.Specifically, we would like to periodically check ROM and RAM. Are there any sample programs for those? [MCU] STM32F412VGT6

UART only works while ST-Link is connected

I'm using an ST-Link broken off from a NUCLEO board to program a custom board with an STM32G4A1 on it. The issue is that UART transmission only seems to work while the ST-Link is connected - probing the line with a scope shows no activity when the ST...

jm-vdai by Associate
  • 1850 Views
  • 2 replies
  • 2 kudos