STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LTDC problem

Hello,i have problem with custom board assembled with STM32F767BIT6. I'm trying to interfacing LCD-TFT DEM 800480K3 TMH-PW-N which is assembled by HX8264E, HX8664B drivers. I'm using RGB888 interface configured via STMCubeIDE filled by resolution 800...

Petr3_0-1710007166195.png Petr3_1-1710007197328.png Petr3_2-1710007231808.png Petr3_3-1710007261454.png
Petr3 by Associate III
  • 2902 Views
  • 2 replies
  • 1 kudos

No trigger of HRTIM burst DMA controller

Hi,I want to update multiple HRTIM registers with a single DMA request on a STM32G474RE. To do this, I am trying to follow this simple Getting started with HRTIM tutorial, which has a section "#To_go_further_about_DMA_burst" on the board "B-G474E-DPO...

PGONOVEA by Associate
  • 1975 Views
  • 1 replies
  • 1 kudos

Resolved! On board SPI to SPI in STM32F207ZGT6

#include "main.h" SPI_HandleTypeDef hspi1; SPI_HandleTypeDef hspi3;   UART_HandleTypeDef huart3;   /* USER CODE BEGIN PV */ char spi_data_tx[1]={'1'}; char spi_data_rx[1]={'0'}; void SystemClock_Config(void); static void MX_GPIO_Init(void); static ...

Store data in internal flash without erasing whole page

Hi, I would like to know method and sample code storing data without erasing whole memory page. I do refer example FLASH_EraseProgram, but i have wrote program that almost finish up the flash memory, if i erase a page, a 2KB page, it will erase my co...

Hollis_K by Associate III
  • 3455 Views
  • 6 replies
  • 3 kudos

Failed to trigger STM32L431 USART1 bootloader via SW

Hi guys,I could set MCU into bootloader mode manually by using PH3/Boot0, but I can't get trigger bootloader via SW... I did check previous posts, but somehow it does not help.HW setup: I have dev board with STM32L431. It has USART1 (PA9, PA10) conne...

Lex by Associate III
  • 1896 Views
  • 3 replies
  • 0 kudos

Resolved! Not a genuine ST Device!

HiI would like to debug STM32F303RDT6 using a combination of Keil and ULINK2.When I start debugging on the target microcontroller (STM32F303RDT6), **Not a genuine ST Device! Abort connection** is output as shown below.We investigated the cause.I foun...

Ukazu by Associate III
  • 8793 Views
  • 10 replies
  • 6 kudos

LORA E5 grove module

Hello,I'm currently sending AT commands to the Grove LoRa E5 module from Seed Studio, when I send commands like "AT," there is no response from the module. I've connected the module to the USART of the STM32L476RG board. If anyone has encountered and...