cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L452 Temperature

bmohandes
Associate

Hi,

How can we extract a correct reading of the internal temperature of the STM32L452 in degree C?

We currently read a number '141' but this is clearly not the CPU temperature which should be 22-28oC

We have followed the general app note on temperature reading https://www.st.com/resource/en/application_note/dm00035957-stm32l1x-temperature-sensor-example-stmicroelectronics.pdf

This does not provide right info.

Is there a correct procedure for extracting this?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome @bmohandes, to the community!

You used AN3964 to refer to an application note that was written for STM32L1.

It is best to take a look at the description of the temperature sensor in RM0394, section 16.4.32. The principle is also illustrated in the example ADC_TemperatureSensor for the STM32L476, which can be found in the repository, either your local copy STM32Cube_FW_L4 in

STM32Cube_FW_L4_Vxyz/Projects/NUCLEO-L476RG/Examples_LL/ADC/ADC_TemperatureSensor

or the online one which can be found here.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.