STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5xx: SPDIF out - how to configure?

I am struggling since days to get "my audio" out via SPDIF (electrical).What I see on scope (there is a voltage divider and cap for DC-free on PC12, Vpp is 0.6V, approx. 75 Ohm impedance):It makes sense - but my SPDIF receiver (a STM32F769I-DISCO boa...

MCU_SPDIF.png
tjaekel by Lead
  • 4370 Views
  • 5 replies
  • 0 kudos

Resolved! ADC Calibration doesn't complete on STM32G0C1RE.

Using HAL_ADCEx_Calibration_Start() to calibrate the ADC. This function always returns HAL_ERROR.Debugging shows its failing after it collects the 8 samples and attempting to disable the ADC is timing out.  (ie.  if ((HAL_GetTick() - tickstart) > ADC...

BrianB by Associate II
  • 9410 Views
  • 11 replies
  • 4 kudos

How to flush cache in CubeF7 Flash EraseProgram example?

In the CubeF4 Flash EraseProgram example (STM32F4-Discovery/Examples/FLASH) there is this section after the erase:/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache, you have to make sure that thes...

osiris81 by Associate
  • 3421 Views
  • 4 replies
  • 0 kudos

stm32l431rct6

I am following the tutorial from https://www.youtube.com/watch?v=I9KDN1o6924&t=384s the tutorial(32F746GDISCOVERY) User manual has showed MicroSDcard_detect is pin PC13.I can not find my pin name of stm32l431rct6 Datasheet for MicroSDcard_detect pin....

Jacob3104_0-1711997870568.png
Jacob3104 by Associate II
  • 1230 Views
  • 1 replies
  • 0 kudos

Storing data in the option byte of STM32 memory.

Hi,1.Can I use option bytes to store the data(eg: Serial number, values storage etc).is It possible if so please share the available resource link/ example for reference. I am using STM32G491RE MCU.I want to write some data in to option byte memory a...

Resolved! STM32L431CCY not reliably booting

I made a little proof-of-concept board for the L431, as I wanted to see what it would take to do a BGA design. I've been able to program is using the STM32CubeIDE, but the board won't boot reliably.STM32CubeIDE v1.13.1Jlink Plus Compact0.1uF Bypass c...

sethkaz by Associate III
  • 1624 Views
  • 2 replies
  • 0 kudos

STM32F756VGH6 problem running 2 timers at the same time

Hi,I am a newbie learning to program STM32 via registers only. I have been doing step after step progress and managed to test and run the led blink program, timer delay, external interrupt etc. So hardware, core clock and other configurations are alr...

Vilius by Associate III
  • 2965 Views
  • 4 replies
  • 1 kudos

Resolved! One pulse with repitition counter

Posted on March 03, 2017 at 08:14 Hi all, I am a newbie developer for STM I am developing an application using the STM32F746 Discovery board and KEIL uVision. I need to output two pulses on GPIO that I will feed to another board. The first pulse ...

0690X00000603i0QAA.jpg