STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HEX file with 32 Byte data line

Hi,my post build command produces the following output with 16 Byte per data line:  :020000040802F0 :1000000000000120E9C00008593D0008CD3D00086E :100010001D3E00081F3E0008213E000800000000B1arm-atollic-eabi-objcopy.exe -O ihex --gap-fill 0x00 --pad-to 0...

Martin42 by Associate III
  • 3843 Views
  • 5 replies
  • 2 kudos

STM32C011F6U7 MCU schematic Reset and programming tool

Hi Guys,I will use STM32C011F6U7 did my devices development, but I can not certain that the schematic is correct or not, is right for NRST part? same time I want to know what tools should I used to download FW to units, 5 pins J-LINK or others 4 pins...

gavin3_0-1712050121861.png gavin3_2-1712050147176.png
gavin3 by Associate II
  • 2154 Views
  • 2 replies
  • 2 kudos

Resolved! Plans for memory scaling in STM32U0

I know the product is new, but are there already some plans on the horizon to maybe increase the flash size and/or have some more intermediate sizes?

OliM by Senior II
  • 1201 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H7 MCU dual processor programming file

Hi, I have a question. I just completed a program for a dual processor MCU, specifically an STM32H745, which has one M7 core and one M4 core. Now I have to organize the production of a hundred cards, and the manufacturer asked me for the .hex file to...

FMass.1 by Associate III
  • 2545 Views
  • 3 replies
  • 0 kudos

Properly add BLE library (.a) to a project

In order to design the Bluetooth Low Energy part of my software, I decided to use BLE Profiles_Lib 3.1.3 Library.There is a few folder inside this root folder (BLE_application, BlueNRG1_Periph_Driver, Bluetooth_LE, CMSIS, cryptolib, hal, SDK_Eval_Blu...

Resolved! STM32F746 QSPI XIP with TouchGFX and FreeRTOS

Hello All, I am very beginner in embedded technology. I would like to learn and implement XIP.Currently I am working on a project which uses STM32F746 discovery board and uses TouchGFX and FreeRTOS. It uses qspi in memory mapped mode to store the fon...

pitbull by Associate III
  • 3238 Views
  • 4 replies
  • 1 kudos

STPM33 spi read issue

I am using STM32 H563 Nucleo board to read the configurational register (address = 0x24) of STPM33 evaluation board using SPI protocol but while debugging the code i am getting random values on each transmission. Firstly i am transmitting an bytes {0...

Dev_Oza_0-1712052899008.png Dev_Oza_1-1712052912298.png Dev_Oza_2-1712052924621.png Dev_Oza_3-1712052938852.png
Dev_Oza by Associate
  • 1418 Views
  • 0 replies
  • 0 kudos

Sometimes HAL_SPI_TxRxCpltCallback() is not getting called.

We are using STM32G4 Series microcontroller for SPI comm. as slave with microprocessor.For SPI TX operations sometimes we are seeing that callback function HAL_SPI_TxRxCpltCallback() is not getting called even though we are seeing that data is transm...

_legacyfs_online_stmicro_images_0693W00000bkHdKQAU.png
PDhar.1 by Associate II
  • 5950 Views
  • 7 replies
  • 0 kudos