STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G491RE QUADSPI ISSUE

Hello,I'm facing a strange issue with the quadspi peripheral.I'm using it to interface with a W25q256jveiq, a quad spi enabled flash chip from Winbond.As long as I use one line SPI or dual I/O mode all works fine.I can access the flash chip with no i...

zeboss49 by Associate III
  • 2538 Views
  • 4 replies
  • 0 kudos

Resolved! Single USB Host to Multiple USB Virtual Ports

Hello,I have an STM32F373 and have successfully enabled a USB virtual com port.I currently send data packets from a PC host to the slave device and include a 'deviceId' in the packet data header.I would  like to support the single PC host communicati...

LMorr.3 by Senior II
  • 7921 Views
  • 9 replies
  • 1 kudos

STM32F103RCT6烧毁

早上好! 在装机生产中STM32F103RCT6芯片能正常工作,成品机器交付客户使用后出现STM32F103RCT6芯片烧毁损坏的情况。成品机器与客户端通讯接口内信号线是直接连接芯片I/O口,客户端与成品机器联合使用,当成品机器出线异常(后排查为STM32F103RCT6芯片烧毁),客户端未出现芯片烧毁的情况。相关直连引脚为【PB3】&【PB4】,PB3做输出I/O量,PB4做输入I/O量。 请问该芯片烧毁的原因可能是哪些?

YANG_3 by Associate
  • 1527 Views
  • 1 replies
  • 0 kudos

Resolved! Write/Read issues with HyperRAM S70KL1282 on OctoSPI2 (STM32H7A3)

I am currently ramping up a new project which has a HyperRAM installed (S70KL1282 - like in the example project of STM32H735G). With the help of this sample project code I can successfully write and read with memory mapped mode from the 16 MB RAM - b...

GS1 by Senior III
  • 3294 Views
  • 4 replies
  • 2 kudos

Resolved! USB-OTG- USB Device Problem

HI STM Team,I am new to STM32 Board. I am using NUCLEO-F439ZI Board. When I was connecting my USB-OTG side to my PC, I will suffer from the "Unknow USB Device" Error, The error screenshot was attached below for your reference . Please Guide me to rec...

Ramachandran1992_1-1714037120515.png

Resolved! STM32F4 Series a Question About I2S

Hi, I am trying to do an application where I am using 2 PDM output digital MEMS microphones to get a stereo sound from them and then play it. My question is when I select I2S as Full-Duplex Master for STM32F407VG it only has 1 SD pin. Should connect ...

mdmrl00 by Associate II
  • 2414 Views
  • 3 replies
  • 1 kudos

Resolved! Tranceiving & Receiving Data with UART on STM32H735G-DK

Dear all,I've been wrestling with a communication glitch that's been causing me some serious headaches. Here's the lowdown: I've got this control board hooked up to a pump, and I've been trying to send commands to it via USART1 on my own STM32H735G-D...

Resolved! STM32F4 SPI high level 5V

Sorry, I have another question to ask everyone. I'm currently using the Nucleo F429ZI with SPI interface to receive 12-bit encoded data from another ADC. The Vdrive of that ADC can provide 3.3V or 5V for driving. However, the high level of the STM32F...

Scarlet_0-1713766357977.png
Scarlet by Associate III
  • 15630 Views
  • 28 replies
  • 14 kudos

STM32F405 ULPI USB3343

Hello Guys,I am new to STM and USB HS but have some experience with PICs and other AVRs. I've designed my own custom board (for a keyboard). So after I generated the USB HID code with STM32cube IDE, I successfully downloaded it to the STM, however, n...

maubla by Associate
  • 1820 Views
  • 2 replies
  • 1 kudos