Hi AllI want write on the SDMMC using HAL_SD_WriteBlocks_DMA system call. The function itself works, the sector on the SD is written, but no callback function (HAL_SD_TxCpltCallback) is called.Did someone experienced such trouble ?Thanks
Hithe RX callback is working, only the TX isn't. I registered the callback in both manners: by the _weak pragma and using the HAL_SD_RegisterCallback, but still only the RX callback works.