STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

G431 - Investigating ADC behaviour depending on clock source

Hi,i am trying to investigate the behaviour of the ADC when measuring a value, where the ADC is triggered from a timer source.In the manual it states, that when the ADC is clocked from SYSCLK or PLL "P", then it would be faster, but when clocked from...

Tobe by Senior III
  • 2901 Views
  • 1 replies
  • 0 kudos

CAN Bus doesn't work in normal mode between two MCUs

Hello,Hope you all doing well..!! I am using two microcontrollers i.e., for transmitting data I have to use STM32F407VET6 and for receiving I have to use STM32F407VGT6 also I have to connect MCP2551 CAN Transceiver. I am transmitting data from one bo...

mr_vineet by Associate II
  • 15286 Views
  • 22 replies
  • 9 kudos

SD card doesn't work with stm32L552ZET6

Hello everyone,I have been using for a long time the stm32L496ZGT6 in a customized PCB with an uSD card module. Never had any problem interfacing the card. Due to the shortage of supply during the pandemic situation I bought a couple of stm32L552ZET6...

tarm123_2-1700225538973.png tarm123_3-1700225605219.png tarm123_4-1700225637176.png tarm123_0-1700225232010.png
tarm123 by Associate
  • 2397 Views
  • 2 replies
  • 0 kudos

Resolved! I can't blink my leds in H755ZI Nucleo board

I bought a NUCLEO H755ZI board, but I can't make the LED connected to GPIOB pin 14 blink, neither with CMSIS nor with HAL, I saw some tutorials and questions here, but nothing solved it, thank you in advance for your help.

Resolved! STM32H7 QSPI Errata

Hi, we see STM32H7 has Qspi errata as below: But we are not sure where to apply the patch exactly. It says "upon reset and upon switching from memory-mapped", mean in reset function, right after or before "HAL_QSPI_Init"?      

DatTran_0-1714074330817.png
Dat Tran by Senior II
  • 3012 Views
  • 5 replies
  • 2 kudos

Resolved! STML496ZGT6P

Can anyone face this issue at STM32CubeMX tool while generating the code. 

sag_0-1714125523019.png
sag by Associate III
  • 1176 Views
  • 1 replies
  • 0 kudos

Resolved! Seeking Advice for Communication on Nucleo-h743zi2 Board

Hello,   I'm currently controlling a motor with the nucleo-h743zi2 board.   I'm sending commands to the motor driver via PWM and reading the encoder's values. I can currently send commands from a PC and receive encoder values through UART communicati...

HMsDobby2 by Associate III
  • 1925 Views
  • 2 replies
  • 1 kudos

GPIO read correct data

Hi there ! I start a project with STM32G031k8. This board i'm gonna make is  a RS485 slave on the pin 4-5-6-7 of GPIOA i put a dipswitch with pullup resistor , and i read in this way: uint16_t Add = ( 0x00F0 & GPIOA->IDR)>> 4 ;  right now my add is 5...

SGian.1 by Senior
  • 2160 Views
  • 2 replies
  • 0 kudos

How to connect microsd card in stm32f407

Hii, I was trying to connect microsd card module with stm32, i was unable to connect with it because the SDIO interface was not available at stm32f407 discovery board. also it support spi communication but not getting how to get with it. can some one...

Shubham08 by Associate III
  • 4984 Views
  • 7 replies
  • 1 kudos