STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! G431RB 32 Bit Timer

I am attempting to set up an encoder on STM32G431RB using Tim 2 which is 32bit but it is only counting up to a 16bit value and going negative. I looked at the register through SFR and only the first 16 bits are active, is there another setting I need...

2.jpg 1.jpg

STM32 ADC3 acquisition twice

I would like to use the ADC3 of the STM32H7 series chip to realize that the voltage is collected once, and then the voltage is collected at a different point (meaning is it necessary to use two channels, because I see several channel choices in there...

hanqingze by Associate III
  • 776 Views
  • 0 replies
  • 0 kudos

SD card memmory support

Hello,Hope everyone are doing well!Can anyone please provide specific numbers?What is the maximum size(GB/MB) of the micro SD card each STM32 device can support?STM32F407VET6 - SDIO interfaceSTM32F745VET6 - SDMMC interfaceSTM32H745ZIT6 - 2 SDMMC inte...

Resolved! Is this normal? CAN bus generates an error frame when waking up.

Here is what I observe:I have an application running that communicates via the CAN bus. With a certain command via CAN the STM32 (STM32F2xx) is put into sleep mode. Thereby I configure the microcontroller to wake up and get an interrupt when activity...

!BBQ! by Associate II
  • 6635 Views
  • 8 replies
  • 0 kudos

ADC does not output intended values

This should be easy but somehow I cannot make it work? I am working with the ADC of my STM23F4 Board trying to read the input from an AC voltage sensor. My previous code was using HAL and it was outputting my desired values (around 2000), but when I ...

Resolved! STM32L4P5RG two OSPI with multiplexed pin not working

Hi :I have a custom board, the mcu is STM32L4P5RG, I also connect Flash W25Q128(OSPI1) and APS6404L(OSPI2) to it.But I can't reset them and hal status always return HAL_ERROR. Can someone help me?The hardware schematic(Sch.png),Clock configuration(Cl...

Sch.png Clock.png OSPI1.png OSPI2.png

Resolved! CAN Frame Repeating, but is received

Summary: I'm seeing a situation where the CAN frames are repeating when they should only be sent once.  However, the receiving device is receiving them just fine.  Details:I'm running an STM32U545 on it's Nucleo Board, and using a simple CAN transcei...

sethkaz by Associate III
  • 13319 Views
  • 18 replies
  • 1 kudos