STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding Volatge Control in STM32L562CET6

Hi all,          I have working on USBPD Sink project in that ,I have been struck in the part of reading the voltage from the STM32L562CET6(Customized Board)before this process I have done the same project in STM32L562E-DK , What I need to do actuall...

nishadh by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

Measure STM32F373 core temperature

Hi,I was measuring the STM32F373 core temperature.It seems that the core is 56°C while the environment is 23°C, no housing.Is the 56°C a reasonable temperature? It looks quite high to me.I used the settings below:

ADC_Temperature.png
BPutt.1 by Associate II
  • 1275 Views
  • 1 replies
  • 1 kudos

Resolved! Mixing HAL and Direct Register Manipulation

Hello. I am writing a code to read ADC data from an AC voltage sensor. I used HAL to initialize ADC 1 and USART2 for checking the values in Putty. However, I would like to use direct register manipulation to send data to USART6 so that it can transmi...

How to use half precision floating variable

Posted on May 22, 2017 at 12:26Hello,I would like to use half precision floating variable in my project but i don't know how. I'm working on a NUCLEO-L073 board that embeds a cortex m0 STM32l073 MCU that does not have any FPU. I'm using the SW4STM32...

How to use Vrefint when Vref+ is tied to Vssa?

Hi,I wanted to use STM32H743 with TFBGA100 package in a new project. Unfortunately this package does not provide Vref+ pin and it is internally tied to Vssa. I don't understand what is the reference source for ADCs and DAC, can I use VREFBUF in hold ...

krom by Associate
  • 1814 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7B3LIHQ and MX25LM51245GXDI00 OctoSPI flash problem.

Hi.I am using STM32H7B3LIHQ MCU, MX25LM51245GXDI00 OSPI flash, IS42S32800J-6BLI SDRAM and 24bit TFT screen. I used the schematic of the STM32H7B3I-EVAL (MB1331) board when creating the scheme. I wrote programs for FMC, OctoSPI and LTDC peripherals us...

Ekran görüntüsü 2024-05-31 160839.png Ekran görüntüsü 2024-05-31 155348.png Ekran görüntüsü 2024-05-31 155618.png
ABURM by Senior
  • 3541 Views
  • 7 replies
  • 1 kudos