STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error: unknown type name 'SPI_HandleTypeDef'

Hi i encounter this error while compiling SPI1 at ST7735.h, i dont understand as this error 'SPI_HandleTypeDef' type was generated by .ioc in main.c already and i had call this statement in ST7735.h. Could anyone kindly help? error: unknown type name...

Resolved! Can't configure DCMI peripherals

HelloI am starting a project with a STM32U585CIU6 and an OV7670 camera module. I want to use the DCMI interface to get the data, and I'm using the Introduction to DCMI to STM32 MCUs document as a reference.STM32U585 datasheet mentions the support to ...

LuizF_Ferro_0-1717415666926.png

STM32G474xx hrtim1

Hi, I have an inverter project designed with stm32g474xx and there is a "h-bridge" topology in the system.Can I create a uni-polar PWM to get three-level output while controlling this topology with hrtim1? Can hrtim1 generate two complementary PWM ou...

Kayhan by Associate
  • 1267 Views
  • 1 replies
  • 0 kudos

DAC trigger by HRTIM

Hi, I need to trigger DAC1 and DAC2 from HRTIM Timer A on a STM32G474. I have set the DAC Sync option inside the HRTIM Timer A settting to generate a DACTrigOut1 event that triggers my DAC1. But DAC has a separate Trigger event that also works for DA...

berait by Associate III
  • 1744 Views
  • 1 replies
  • 0 kudos

Bootloader on STM32H503RB via USB

We wish to bootload a STM32H503RB using USB. This works on the NUCLEO-H503RB, but after resetting the processor on our PCB with BOOT0 high windows reports "Device Descriptor Request failed".AN2606 states that CRS is enabled for the DFU to allow USB t...

CWedg.1 by Associate III
  • 5023 Views
  • 8 replies
  • 0 kudos

Unable to configure Ethernet as RMII

Hello Team, We are prepared our own board for Ethernet Configuration in STM32H745ZIT6 Board then configured peripherals what we need to use in ethernet after configuring ioc file while debug mode every time it will go error handler when it initialize...

ggowd.1 by Associate III
  • 4942 Views
  • 4 replies
  • 0 kudos

FMC timing calculation for NAND Flash

Hi Team,       I have gone through few documents and application notes for considering timing calculation for FMC to NAND, but still i did not get much understanding on this. Can anyone make me to understand how we need to calculate comspace, attribu...