STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IOselect option in STM32H563 is not working

I am trying to use second half of OCTOSPI pins in single memory mode by setting MSEL bit for QUAD SPI communication with Flash memory. Even though i set the MSEL bit to send the data through 7 to 4 pins, still data is going through the 3 to 0 pin onl...

Nagarajan by Associate III
  • 2552 Views
  • 5 replies
  • 0 kudos

Error with Step one opening file example

Upon selecting the directory:C:\Users\myname\STM32Cube\Repository\STM32Cube _FW_L4_V1.11.0\Projects\NUCLEOL476RG\Examples_LL\ GPIO\GPIO_InfiniteLedTogglingI am unable to see the project file:GPIO_InfiniteLedToggling\SW4STM32 \STM32L476RG_NUCLEOAlso, ...

ks12345_0-1717506284281.png
ks12345 by Associate
  • 1123 Views
  • 1 replies
  • 0 kudos

Resolved! external RAM for stm32h753zi

Hi, my program required a large amount of RAM memory, how can i know which external memory i can choose? and which peripheral is dedicated for this? 

Ditzhak by Associate III
  • 2715 Views
  • 4 replies
  • 0 kudos

ADC polling of multiple channels

Hello,After setting up a 4 channel read with DMA, I ran into the problem, that the value of the internal temperature sensor seemed to not change at all. The values of the read out potentiometer however were plausible.So I wanted to check all used cha...

Resolved! HAL_I2C_Mem_Write_DMA issue

Hi There,I have searched a lot about the  HAL_I2C_Mem_Write_DMA problem and seems like i have not found anywhere else this issue has been solved.Can anyone contribute if someone has solved it. Thanks

Resolved! STM32h7b0 - System memory bootloader AN2606

Hi, I'm having issues on our custom board jumping to the system memory bootrom.Likely i have a software issue but would like to clarify the system memory address for the bootloader. This is usually listed in AN2606 but there is no explicit mention of...

Regarding Volatge Control in STM32L562CET6

Hi all,          I have working on USBPD Sink project in that ,I have been struck in the part of reading the voltage from the STM32L562CET6(Customized Board)before this process I have done the same project in STM32L562E-DK , What I need to do actuall...

nishadh by Associate
  • 807 Views
  • 0 replies
  • 0 kudos