STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32 microcontroller selection.

Hi all Thanks in advance.Can some one help me to select an stm32 chip which have 4 PWM channels , 4 analog out and in 3X3 qfn package? I attached a sample product. Kindly help me to select some more similar products.

ArunPR by Associate
  • 5551 Views
  • 1 replies
  • 0 kudos

Resolved! Dual CAN STM32F105

To implement a "bridge" devise between two independent CAN buses, the STM32F105R8 chip was chosen. From the specifications it follows that it has 2 CAN buses, but going deeper into it I realized that they share a lot of resources among themselves.cou...

YRakh.1 by Associate II
  • 3180 Views
  • 4 replies
  • 4 kudos

Resolved! Integer overflow modes on Cortex

Hello,I am dealing with fixed-point arithmetic calculations on STM32G0.To avoid integer overflow risks I have scaled properly all the values involved in calculations, but a mistake can be always possible...On Texas Instruments DSPs, I have the possib...

CTabo.1 by Senior
  • 2899 Views
  • 4 replies
  • 2 kudos

Resolved! add offset for application start address

Hi,I've ran into an issue which is about start address of an application. I'm using an own bootloader to switch between two different applications. For the application I changed the start address in FLASH.id file to 0x08040000. That works perfectly f...

STM32L496 I2C Reading Error

Hello:  This is weird problem. We have a STM32L496 system that handles multiple I2C devices through its three I2C buses. The I2C#1 (1MHz) has 10 NXP devices, #2 (400kHz) has 4 TI TMP117 chips, and #3 (400kHz) miscellaneous devices including other TI ...

WQ by Associate III
  • 1792 Views
  • 0 replies
  • 0 kudos

Password for USB Device

I am using STM32F4 MCU in USB device MSC mode with data stored on SD card. I have also standard 16X2 LCD & Membrane keypad connected to MCU I want to make interface where once USB device is connected to laptop, the data is showed on laptop after ente...

Nico3 by Senior
  • 1160 Views
  • 3 replies
  • 1 kudos

Floating point calculation in STM32L431CBT6

Dear all,I am having some issues with precision of floating point calculations with STM32L431CBT6.As one can see that when I do floating point calculation I am getting 1.23000002 instead of 1.23.Can anyone suggest more efficient and accurate way to d...

DKhan1_0-1718037438449.png
DKhan.1 by Associate II
  • 5040 Views
  • 6 replies
  • 6 kudos

Which boot should I use on my L476?

I'm looking for a simple solution to update firmware on my application developed on a STM32L476, with the minimum effort.As far as I understood this chip already has a boot on it that allows to get data via UART1 and a proprietary protocol from STM.I...