STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Imprecise error flag after writing to the flash

Hi experts,I'm adding to my existing code (that runs on a STM32F105) a function to store a word in the flash.I basically copied the code from the official example based on the HAL libraries, here my function:uint32_t FLASH_Write_Data(uint32_t StartPa...

aga by Associate III
  • 9432 Views
  • 18 replies
  • 7 kudos

Resolved! Speaker output in STM32H563ZIT6

HI,I would like to use the speaker output on the STM32H563ZIT6. I reviewed the wiki, but there aren't any references about how to play audio with the speaker output. Is it possible to enable this output to play audio?Does the STM32H563ZIT6 have built...

EXTI15_10_IRQHandler; interrupt; PE13

Might need your help to solve this issue. Thank you. Background: 1. I have a 1 Hz signal, and I'd need this signal to trigger interrupt. 2. Use GPIO as interrupt. 3. Using STM32CUBEMX to generate codes. 4. STM32F769I-EVAL board. 5. Already successful...

uNavi by Associate II
  • 2990 Views
  • 3 replies
  • 0 kudos

Can't pull up a GPIO pin set as AF QSPI I/O

Hi,I am working on a project on STM32H750. I set up the QSPI I/O pins on PD11, PD12, PD13 and PE2. Because PE2 (IO2) also serves as the WP# pin for the external flash, I would like to set it to have an internal pull-up, so the GPIO definitions are li...

ZhiFeng by Associate II
  • 2237 Views
  • 4 replies
  • 0 kudos

Resolved! Can peripheral-to-memory or memory-to-memory DMA be transfers be configured to substitute for lack of peripheral-to-peripheral features in the Cube toolchain?

I need to load the TIM1 CCR registers into the DAC1 outputs on an STML432KC. I have this working with the line DAC1->DHR12R1 = TIM1->CCRx executing in a loop. I'd like to substitute with DMA. Others have suggested that I can do this with the availabl...

KHarb.1 by Senior II
  • 3950 Views
  • 8 replies
  • 0 kudos