STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to set Adc for maximum rate

I have design  pcb for Stm32H723VGT6 ( 100 pins  TQFP )  my job is read adc 12 bit and transfer over usb to PC  . i have set sysclk to 550 MHz and ADC clock to 64 MHz  so i got sample rate to 1.3 Msps but mcu are hot. So i have sysclk to 400 and ADC ...

tawat25 by Associate
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! STSPIN32G4 and PC13-PC14-PC15 for LED Indicators

Good morning,In regards to the current limit placed on the PC13-PC15 pins of the STM32G431VBx3 that is used as the basis of the STSPIN32G4 (and whose datasheet is referred to multiple times in the STSPIN's), the '431 datasheet has the usual low-power...

MLange_0-1719568668520.png
MLange by Associate
  • 1742 Views
  • 1 replies
  • 2 kudos

Resolved! STM32F407 MCU Maximum Voltage Input

Hi AllMaximum input voltage for this series of MCU per Table II of the datasheet is specified to be 4.0 VDC for all pins other than five-volt tolerant. Table 12 specifies the maximum injected current for all pins other than five-volt tolerant to be +...

IKhan.2 by Associate II
  • 4788 Views
  • 5 replies
  • 1 kudos

Resolved! Problem with UART interrupt

Hi,I have two MCU communicating with each other via RS485. It's a very simple code one MCU send a data to other and the other is trying to receive this. With MCU2 code everything is fine. It sends data like it should be.Problem is with MCU1 code. Whe...

Raf_al by Associate III
  • 5981 Views
  • 13 replies
  • 5 kudos

Resolved! FMC memory in fmc display

hello, I have a display configured for FMC but I would like to add a framebuffer to the RAM memory, unfortunately the MCU memory is not enough (the display resolution is 480x800) so I have to add external RAM. My question is how to do it since I am a...

how to program the option bytes within firmware

Hello,After reading the following threads:How to program STM32 Option Bytes with the HAL API - STMicroelectronics CommunityWhat are option bytes in STM32 and how do I use th... - STMicroelectronics CommunityProblem with option bytes set from program ...

KoSt by Associate III
  • 1085 Views
  • 0 replies
  • 0 kudos