Skip to main content
Melgh.1
Associate II
February 5, 2024
Question

mapping multiple * IP addresses to one Ethernet interface (LWIP)

  • February 5, 2024
  • 5 replies
  • 3799 views

Hello,

I'm attempting to bind multiple IP addresses to a single Ethernet port using different struct netif logical interfaces. My current implementation does not works for the both IP addresses

Seeking guidance or resources on the correct approach. Any insights appreciated.

Thanks,

Melgh1_0-1707141797573.png

 




This topic has been closed for replies.

5 replies

Lead II
February 6, 2024

How can an IP receiver have several different IP addresses?

What you are looking for is "promiscuous mode":

https://en.wikipedia.org/wiki/Promiscuous_mode

An IP receiver might use a HW table to filter MAC addresses, IP addressed (using a Hashing Table).
To assign different IP addresses to a network device, in order to listen to both, sounds impossible to me.

Melgh.1
Melgh.1Author
Associate II
February 6, 2024

in the world of Networking when one interface have more than one IP is called IP aliasing and is a very common practice

Andrew Neil
Super User
February 6, 2024

@Melgh.1 wrote:

My current implementation does not works for the both IP addresses


What do you mean by that?

  • Neither works?
  • only one works?
  • other??

Do you have it working with just one address?

 

Use this button to properly post source code - as text, not an image:

AndrewNeil_0-1707212479217.png

 

To get that extra row of icons, press this button:

AndrewNeil_1-1707212479219.png

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Melgh.1
Melgh.1Author
Associate II
February 6, 2024

Both are not working,
but one works if you deactivate one of them:

//ethernetif_input(&netif);
ethernetif_input(&netif_0);

 

 IP4_ADDR(&netif_ipaddr, configIP_ADDR0, configIP_ADDR1, configIP_ADDR2, configIP_ADDR3);
 IP4_ADDR(&netif_netmask, configNET_MASK0, configNET_MASK1, configNET_MASK2, configNET_MASK3);
 IP4_ADDR(&netif_gw, configGW_ADDR0, configGW_ADDR1, configGW_ADDR2, configGW_ADDR3);

 IP4_ADDR(&netif_ipaddr_0, configIP_ADDR0_0, configIP_ADDR1_0, configIP_ADDR2_0, configIP_ADDR3_0);
 IP4_ADDR(&netif_netmask_0, configNET_MASK0_0, configNET_MASK1_0, configNET_MASK2_0, configNET_MASK3_0);
 IP4_ADDR(&netif_gw_0, configGW_ADDR0_0, configGW_ADDR1_0, configGW_ADDR2_0, configGW_ADDR3_0);



 lwip_init();
 snmp_example_init();


 netif_add(&netif, &netif_ipaddr, &netif_netmask, &netif_gw, &enet_config, EXAMPLE_NETIF_INIT_FN, ethernet_input);
 netif_add(&netif_0, &netif_ipaddr_0, &netif_netmask_0, &netif_gw_0, &enet_config_0, EXAMPLE_NETIF_INIT_FN_0, ethernet_input);


 netif_set_default(&netif);
 netif_set_up(&netif);

 netif_set_default(&netif_0);
 netif_set_up(&netif_0);






 while (1)
 {
 /* Poll the driver, get any outstanding frames */
 ethernetif_input(&netif);
 ethernetif_input(&netif_0);

 sys_check_timeouts(); /* Handle all system timeouts for all core protocols */
 }
GreenGuy
Senior III
April 3, 2024

How many interfaces have you configured for?  By default the NetxDuo library defaults to 1.