STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G474E EVAL1 Demo SD Card issue

Hello,I tried to execute the demo for the STM32G474E EVAL1 explained in this document : STM32CubeG4 STM32G474E-EVAL demonstration firmware - User manual.But, I have an error when the board tries to display the pictures which are on the SD card.I got ...

twinest by Associate II
  • 13289 Views
  • 18 replies
  • 2 kudos

Resolved! USART RTS vs CTS

Hi,I would like to connect my Sequans GM02s iot module to my Stm32L4 mcu via uart. Would the RTS Signal from the iot module connect to the CTS signal from STM32L4 or vice versa?

Nick102 by Associate
  • 1290 Views
  • 1 replies
  • 0 kudos

Resolved! LPTIM1 ISR never cleared STM32L031G6

Hello, I would like to know if anyone has already encountered this problem. I have an LPTIMER configured with an ARR Match interrupt at 100ms I also want to enter my interrupt every 10ms so I added an interrupt in compare mode at 10ms.I have 2 questi...

Resolved! Compatibility between NUCLEO H743ZI2 and H753ZI

Hello,For my project I am working on two nucleo board H743ZI2.Unfortunately, during an experimentation one of the boards ceased working (LD4 and LD6 red). Maybe a short circuit, I don't know.Anyway I tried to purchase a new NUCLEO-H743ZI2 but it seem...

Kévin by Associate III
  • 2731 Views
  • 2 replies
  • 2 kudos

STM low price 4xI2C, 48 pin

Hello,I am looking for STM with the following features:- 48 pin (could be 64 pin only if BGA)- 4 I2C interfaces- 1 ADC channel- most important: lowest price possibleCould somebody suggest several P/N I could check? Adam

adams1 by Associate
  • 1019 Views
  • 1 replies
  • 0 kudos

ETH_REF_CLK (PA1) noise / crosstalk on ADC1_IN0 (PA0)?

Hello,Has anyone seen ADC noise generated by the 50 MHz RMII clock (PA1) affecting the measurement on ADC1_IN0 (PA0)? (approximately 100 codes in 4096).If so does anyone had a fix to suppress it?All other ADC channels used do not have the same level ...

###### by Senior II
  • 2652 Views
  • 5 replies
  • 0 kudos

Usage of decoupling capacitor in STM32H503KBU6

Hi,      I am currently using STM32H503KBU6 MCU (32 pins). For my project the space in PCB board is critical. I have placed a LDO, Level translator, voltage supervisor and along with their associated passives in a 10mmx16mm PCB board. Now I still nee...

bhavan_kumar_0-1719978260721.png bhavan_kumar_1-1719978267514.png