User Activity

HelloI would like to confirm with you the power on reset behavior of TS334.When I power up the comparator, I see a high level impulse during power on.I guess there is a power on reset behavior of TS334. In the following figure, the blue curve is the ...
When the comparator input pins exceed V+ or GND, will the output of the comparator has phase-inversion?Thanks!
HelloCould you share some detail of STM32U585 temperature sensor information?When do the calibration in plant, how to guarantee the junction temperature of the chip? Do you perform the calibration with bare die or with package?How about the linearity...
HelloI use the embedded Op Amp in STM32U585VIT3Q to charge a 47uF capacitor.The input of the Op Amp is connected to the output of DAC. The voltage level is 3V.So you can see when the Op Amp begin to charge the cap, the peak current is quite large.I w...
HelloIn my application, I use the DAC of the Micro to charge a capacitor(47uF). When the micro is power off, the voltage on the capacitor start to discharge with a high impedance resistor(6.8Megohm). I want the leakage current of the Micro I/O small ...
Kudos from
Kudos given to